Experimenting with Vibration Sensors - Machinery Safety Blog#11 (Review & final thoughts)
Posted by dwinhold in Experimenting with Vibration Sensors on Jan 14, 2021 3:04:00 PMExperimenting with vibration sensors – Machinery safety Blog #11 (Review & Final Thoughts)
For those of you that have read my blogs, you might have a good idea how my review and final thoughts will be.
Review:
From the day I received the KEMET Vibration Sensor I had a good idea that this challenge will be fun. My proposal was to use the sensor to check machinery vibrations and shut it down when the vibrations were too much. I was originally going to use the Nucleo-144 but with a lot more experience with the Arduino, I used an Arduino Mega. As I started to create the program to run the vibration sensor, I saw a need to expand my original idea.
This is a basic timeline of my code:
- Write code to read the sensor.
- Add code to shut down machine when the vibration was too high.
- What is too high?
- How do we tell the relay switch if we don’t know what is too high?
- Calibrate the sensor?
- So, add code to calibrate the sensor (get average from 15 checks of the sensor over 10 seconds)
- I need to see the vibration output away from the computer.
- Add LCD display, problem solved.
- Make it so you can set your own shut down limit.
- I did this by adding a button. When you are prompted to set the % over average to shut down, you press the button until you reach the number you want to use.
So far so good, this all worked great (See blog #8). At this point my proposal is complete; machine shuts down when vibrations meet the parameter. But this wasn’t enough for me. This sensor is incredible, I need to experiment more. I guess it is time to change the code a little.
- Needed to write code to run a different program so I can check the vibrations without the sensor shutting down.
- After starting to write new code I had a thought, give the user a choice of which program to run instead of having to keep loading different programs.
- Delete new code; add to original code with buttons to choose which script to run.
- Oh no, new programming territory, time to learn. (Proof, you’re never too old to learn new things.
- It was quite easy, create functions!!
- Now that works great, I want to see a graph of the output.
- Solution, add a oscilloscope to my Arduino. Not good solution, missing to many electronic part to make it work.
- New solution, Arduino IDE has one built in. Since all the rest of my experiments were at the computer I had the IDE show me the graph.
- Like I said, to much fun. Code complete.
The code is uploaded in my blogs for anyone who wants to see. The KEMET Vibration Sensor is the best I ever had the privilege to use and the one I have had the most fun with. I am still experimenting!!
Final thoughts:
I am so thankful to have been chosen to be part of this challenge. The sensor is incredible; the sensitivity picks up the slightest vibration. With the machines, the calibration averaged 513Hz; I set the sensor at 5% shutdown limit (538.65Hz) which I found was the adequate limit. Since the code was written to calibrate the average then add the 5%, made it work on any machine.
I could keep talking about how much I love this sensor and its abilities, but I would just be repeating myself.
I really hope we can have other challenges with different KEMET sensors.
Thank you KEMET for sponsoring this challenge, you made the past 2 months very enjoyable through these tough times. Your VSBV20 Vibration Sensor is incredible and I will tell everyone about it.
Thank you Element14 for everything you do for us and hosting these challenges.
Thank you Element14 community for being the best group I belong to!!
My Blogs:
Experimenting with Vibration Sensors - Machinery Safety
Experimenting with Vibration Sensors - Machine Safety Blog #2
Experimenting with Vibration Sensors - Machinery Safety Blog 3 (Information)
Experimenting with Vibration Sensors - Machine Safety Blog#4
Experimenting with Vibration Sensors - Machinery Safety Blog #5
Experimenting with Vibration Sensors - Machine Safety Blog #6
Experimenting with vibration sensors - Machinery Safety (Sort of) Blog #7
Experimenting with Vibration Sensors - Machinery Safety Blog#8 (It's working)
Experimenting with Vibration Sensors - Machinery Safety Blog #9 (More photos)
Experimenting with Vibration Sensors - (Not) Machinery Safety - Blog #10
Thank you,
Dale Winhold
Comments