Skip navigation

Forget Me Not Design Challenge

4 Posts authored by: bose
First an update on the PCB I mentioned in my last post. The PCB came out really well and was useful in fitting the sensors. Below I have also attached the pictures of the STM330 fitted onto these boards. Here are pictures of the PCB on both sides. In case any one wants the design drop me a PM I will send them with the gerber. Although the PCB was great but I missed on one point. The 2MM connector that were suppose to hold the TCM320C were shorter than required. The TCM320 has 16 pins but o ...
bose

SCHO Addon

Posted by bose Aug 25, 2014
I have designed an PCB holder for the EnOcean Sensors. This PCB would help to mount the sensors on the doors, windows and other desired locations. Thanks to EnOcean for the Additional PTM200C module, Rockers cases , STM320C enclosure and the connectors. Actually I missed to order the 1.27mm pitch connectors, so EnOcean sent me a couple of spare 1.27mm connectors. They also sent me a small enclosure for the STM320C this helped me to design this PCB and fit the first sensor on my door. Thank ...
bose

SCHO Parts

Posted by bose Aug 13, 2014
I have already received some of the parts. Actually all the parts in my additional part list but not the Raspberry Pi B+ and the TBS1202B-EDU Oscilloscope. Here are a couple of pictures of the boxes and modules: Assembled the EnOcean Pi on one of the older Raspberry Pi boards.   The Sensor Kit Parts (315MHz):   TCM 320C TRX Module to act as Actuator Receiver : Connected using a 2mm Pitch connector on the board.   Raspberry Pi Camera and Web Server Raspberry Pi: This wo ...
bose

SCHO Design

Posted by bose Aug 13, 2014
Hello Everyone,   First of all apologies for not being able to make up my progress post for past two weeks. Although I have been doing a lot of prototype building stuff in the back end which I will summaries in this post. Let me first start with the idea. SCHO – Safe Connected HomeAn IoT based automation and energy efficient monitoring  This project is designed to provided connected control of house and security monitoring. Utilizing the energy efficient wireless network of se ...