Skip navigation
HW Chapter 2 video: Xilinx Embedded Tool Flow The presenter first went over the different Vivado Design Suite editions: WebPACK is free and supports the common Zynq devices that are found on most development boards (7010 and 7020), and the more expensive HL System & Design editions which support additional features like Partial Reconfiguration & System Generator for DSP. The next slide summarized the typical workflow of Zynq Development. The hardware designer uses Vivado, the IP Integra ...
Introduction  Path to Programmable is a training course for Programmable SoCs, like the the Xilinx Zynq-7000 All Programmable SoC. As many others have pointed out, this isn't a typical FPGA/HDL course, since the training material focuses less on the digital design/FPGA aspect, but is more about using Xilinx tools (like IP based design etc) - many of which will be relevant for other non-SoC FPGAs in the Xilinx portfolio and some might apply only to Zynq (PS-PL interconnects etc.). In line ...