Skip navigation
In this Video,I have shown the Step by step Procedure of working on Xilinx SDK for Developing Software Application for Minized and also given the Details pertaining to functionality of various blocks and  Necessity of various files.   It Answers to Aspects relating to: What do Hardware Definition File contains? Necessity to Import .hdf file? How SDK provides the Hardware Design Details to the Software Developer ? How Software Programmer can used Memory Mapped Register ? Why and H ...
Hey everyone,   ZynqHW_2017_lab_3_v13.pdf   In lab 3 we will start discussing the other Zynq blocks in detail. The lab starts with introducing the selection of boot device. The QSPI memory interface (Quad Serial Peripheral Interface) is a SPI (another asynchronous serial communication protocol) module which has a memory mapped register interface, which allows direct interface for accessing data from external SPI devices and thus simplifying software requirements. The bootup of the QS ...
To control my camera module, I'm going to use a X-Y gimbal made from RC servos. I will run the servos from the MiniZed. To do this, I have modified the code from the IP training to run two RC servos instead (and addition to) the PL leds. The new Vivado Block Design is as follows: I added another instance of the IP PWM_w_Int, and connected it to PL_LED_G The new address of the second PWM channel (Green LED) is 0x40002000: The green and red PL LED pins are also available on the Arduino ...