In this Video , using the Minized Board based on Xilinx Zynq :

1.)We Develop Application which Blinks PS LED controlled with PS Button by using Interrupts instead of Polling and We create a Changing Pattern in LED Blinking

2.)We Develop PL LED Blinking Application by using the GPIO driver in PL based on the Hardware Design

3.)We can see how to use Example Programs to develop our own Interrupt Based Applications.

4.)We see the possible Pitfalls and Bugs we may encounter when using example Programs

5.)We will also see how the Hardware User Guide File is needed to analyze the Validity of our Program

6.)We will also see how a bug in simple Input and Output pin assignment can cause the Application don't perform as desired

7.)We will see about Interrupt Handlers

and much more...

 

 

-----------------------------------------------------------------------------------------------------------

Download Resource Files from  Github:

https://github.com/uElectron/minizedSDK