Download Resource Files from  Github:

https://github.com/uElectron/minizedSDK

======================================================================

In this Video , using the Minized Board based on Xilinx Zynq :

1.)We review about the First Stage Bootloader  and its requirement.

2.)We then Generate a Boot Image for QSPI using Bootloader,Bit Stream and Led Blinking Application using Boot Gen provided in SDK.

3.)We then Flash the Boot Image Onto the Minized QSPI Board .

4.)We then set the Boot Switch to "F" (Flash) side instead of "J" (JTAG)side and connect the Board to the Power Socket using Auxilary Power Port.

"Bingo ! We Got Off the Shelf Led Blinking Program on our Board."

 

This video is Based on my Previous Lectures of "Software Application Development for Minized Board on Xilinx SDK" playlist :

Path to Programmable