• SW Application Development - Hello World with UART on Minized Board

      In this video we can see how we can implement any Peripheral functionality into Our Application, it is explained it by means of UART peripheral as an example. We can see how the code is Implemented, how to se...
    Profile Photo
    last modified by mu.udhay
  • Path to Programmable Blog 4 - Adding a PL Peripheral & using PS DMA

    In the preceding posts, we had a quick look at what Zynq-7000 is (Path to Programmable Blog 1 - Getting Started), the workflow (Path to Programmable Blog 2 - Xilinx Tool Flow & Getting Started with Zynq-7000) and ...
    Profile Photo
    last modified by avnrdf
  • Path to Programmable: Final Projects and Graduation Awards

    In 2018, we had our first Path to Programmable class. I described how the class was conceived by the element14 team, and why we are committed to providing element14 members training on programmable logic devices in a ...
    Profile Photo
    last modified by rscasny
  • 06 - "The Projekt"

    Hey Everyone, After spending a few nights on this - I have decided my project is to be a "microphone" based project. Sounds simple enough right ? ( ) As I progressed, it has later on branched out to be something els...
    Profile Photo
    last modified by nixiefairy
  • Summary of Module 2 Path to Programmable ZYNQ SW blogs

    The list of the step by step zynq software development blog learnings and projects are as below     Topics in the minized ZYNQ software development Link to the minized software development blogs Introductio...
    Profile Photo
    last modified by snidhi
  • Working with DMA through AXI between DDR and PL BlockRAM

    Hello Everyone, My peers in Path to Programable have Done Great work in giving step by step procedure to implement DMA transfer so Why Reinvent the Wheel , I take a different approach. I will try to present a vivid p...
    Profile Photo
    last modified by mu.udhay
  • Path to Programmable: Course Syllabus

    Path to Programmable About Training Project | Course Syllabus | Application Instructions | Mentors | Terms & Conditions | Trainees Announcement   This is NOT a Design Challenge. See Special Note below. ...
    Profile Photo
    last modified by pchan
  • In zturn board usb otg to access pendrive to see the result console window by using uart

    In zturn board usb otg to access pendrive to see the result console window by using uart...Is it possible please help me
    Profile Photo
    last modified by gudellykavyasree
  • Driving a Laptop LCD using an FPGA

    In Path to Programmable Blog 7 - Trying out a PL-only VGA design & Path to Programmable Blog 10 - MiniZed does DVI/HDMI, I used the MiniZed that was sent to the Path to Programmable challengers to generate VGA &am...
    Profile Photo
    created by rscasny
  • [PP-22] Gamma radiation measurement with MiniZed

    1. Introduction I have a really nice sensor module called GDK101 which allow to measure a gamma radiation in range up to 200 usV/h. This sensor have really simple communication interfaces: I2C or UART. There is also ...
    Profile Photo
    created by rscasny
  • Final Words and Future Opportunities on the Path to Programmable: Summary, Projects, Conclusions and Thank Yous

    About a year ago (on an impulse) I began the discussion Re: What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)  The discussion was meant to inspire a spirited conversatio...
    Profile Photo
    created by rscasny
  • Path to Programmable Blog 10 - MiniZed does DVI/HDMI

    Continuing (off the course of the syllabus) from where Path to Programmable Blog 7 - Trying out a PL-only VGA design left off, I decided to try generating a HDMI/DVI video signal.   HDMI/DVI 101   VGA is a...
    Profile Photo
    created by avnrdf
  • Project - Minized as Web Server with Video Hosting on USB Pen drive

    Intro: I build this project mainly out of my need to watch videos on multiple devices. I use to see few lectures on my Home Laptop , Some on my Tab and very few on my mobile ,hence i maintain a copy of videos on all ...
    Profile Photo
    last modified by mu.udhay
  • Running Webserver on Minized Board

    Open video

    Profile Photo
    created by mu.udhay
  • Path to Programmable Project Blog

    Overall Impressions   Well, I'll have to say this was a very interesting process. There were some delays, which collided with my schedule, there were some bumps, and there were some unexpected surprises. All of ...
    Profile Photo
    created by mconners
  • FPGA - 05 - Hardware debuggin and the intro to TCL II

    Hey everyone, And just like that we have reached the end of the lab manual series.   Zynq_2017_4_lab_8_v12.pdf   The lab starts off from where we had left off earlier. Just to recap - We now have a bitst...
    Profile Photo
    created by nixiefairy
  • Watchout for I2C in Minized to talk to On Board Temperature and Accelerometer

    I made this post because i found the example code provided in SDK for I2C is not meant for Minized , if it is not realized then it would be frustrating in figuring it out. I am not going to show how to modify that gi...
    Profile Photo
    last modified by mu.udhay
  • Path to Programmable - Project update - I made something!

    Well - I finally managed to do it! I have created a basic project based on the lessons from the training.   About:Through Avnet, Xilinx and Element14, a training program to learn about the Zynq 7000 platform w...
    Profile Photo
    created by aspork42
  • FPGA - 04 - Testing the BRAM and Intro to custom IPs !

    Hey folks, ZynqHW_2017_4_lab_6_v12.pdf  So let's continue our arduous journey through the lab manuals. Boy, aren't things spicing up a bit? So the first part of lab 6 shows us to import our SDK files done from ...
    Profile Photo
    last modified by nixiefairy
  • Path to Programmable: Trainees Announcement

    Path to Programmable About Training Project | Course Syllabus | Application Instructions | Mentors | Terms & Conditions | Trainees Announcement   Welcome to the Path to Programmable Trainees Page! Our Pa...
    Profile Photo
    last modified by pchan