Skip navigation
Previous posts for this project: Sci Fi Your Pi: PiDesk - Project Description Sci Fi Your Pi: PiDesk - Project Update #1 Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2 Sci Fi Your Pi: PiDesk - Project Update #2 Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board Sci Fi Your Pi: PiDesk - Project Update #3 Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot Sci Fi Your Pi: PiDesk - Project Update #4 Sci Fi Your Pi: PiDesk - Project Update #5 Sci Fi Your Pi ...
Introduction At the actual date the first part of the project is closed: machines are assembled in the box, powered and the entire architecture has been set about 95% accordingly with the initial design. The only plus is the introduction of a fourth PI as the Cirrus audio board it is very difficult to match with any other hardware implementation on the same device so the PI hosting the Cirrus will only work in conjunction with the Bitscope module via the USB that is used in reverse mode. I mean ...
Introduction In the Meditech container there is a variable number of devices working at least at two different voltages: 5V and 12V. In this prototype version the definitive powering system has been moved to the bottom of the priorities due the restricted deadlines and the need to have an experimental unit before a final decision: battery type, charging type, power consumption etc. Just for this reason the power will be granted by a common ATX switching power supply. This implies a couple of con ...
Starting from the selected box that will host the Meditech prototype components the first step has been to prepare the container to host the prototype components. First of all the setting of the cooling fan. The following image shows the general idea on how to use one of the two sides of the box. The other side will contain the default probes, accessories etc.   A modular system To keep the system totally modular, every specialised device (based on the Raspberry PI) is hosted on one of ...
The prototype container is arrived today, just waiting to be adapted to host the Meditech components.     It is almost compact and has sufficient space to share all the components, the power unit (in the base) and one of the two sides will contain probes and accessory. For now the decision is to posticipate the question of the battery powering and charger system. Just to remember, the project will include: solar cell, external domestic power charger and car power charger. For this ...
Since my last post I've made some good progress on setting up communication between the various Raspberry Pi computers over MQTT. I got a case in the mail for my RPi 2 and that bugger is now sitting in the living room with a network cable plugged directly into the cable router. At my desk I have the other two RPi's that make up the brains of the pizza carrier.   PiFace CAD is running on my old RPi model B and the Xtrinsic board and GPS module are on the Model B+. Both have their own wifi d ...
Previously: Sci Fi Your Pi - Prince Dakkar's patent log taking chart compass Sci Fi Your Pi - Prince Dakkar's patent log taking chart compass - Functional Design   Route Selection and Indication One of the main elements that makes up the design is the indication of the route that will be taken from the current location to reach the destination. This works in two parts the selection of the route and then the indication on the map.   To select the route I wanted to use some suitably ...
May 23 2015 Day 30 Sound Test I have been working diligently on some of the sound bytes I intend to use and the necessary scripting involved triggering the sound bytes at the appropriate time during sensor reading activity. Scripts will be commented appropriately when modified specifically for the Picorder operation. Final code and documentation will be provided later as the project nears completion.   In the accompanying video sound test, I am using the previously dissembled stereo sp ...
Abstract Why another tutorial Pi Camera Python Module Pi Camera Template Capture a timelapse Conclusion Abstract The project proposed has a subsystem which can use the image processing capabilities of the RPi to get commands visually which can be transmitted to various devices over the network. In the previous post (http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/16/project-virusweek-2-getting-started-with-opencv-and-rpi-camera) ...
The HDMI Monitor As I mentioned in some post before, the initial idea to use a separate tablet as display unit has been expanded and simplified, using an LCD display integrated with the device. With the advantage to use the external smartphone or tablet as the access point for tethering only. The two images below shows the prototype display. It was already available so it is sufficient to make tests but it is 4:3.   The used monitor is a non-standard HDMI; I mean that it supports the H ...
My kit have arrived (yes, almost 45 days, thats a con. to live in Brasil), SO, i will keep it updated weekly, any news, in the next posts...   Tks all, and good luck to all of us ...
Hi everybody   Is time for a new step in Cybernetic Interface development - audio interface configuration. Because RaspberryPi lacks a microphone input, which I need for my project, I had to add and configure an external USB sound card. Due to space constraints I picked the smallest I could find,  Konig 3D Sound, based on C-Media CM108 Audio Controller. It worked from the first try, plugged directly in RPi USB port or in USB Hub. Configuration and testing steps are listed bellow ...
Week 3 Blog This week has seen more Python coding to produce menus and test out the capabilities of the PiFaceCAD. but it is not elegant enough to share just yet.  I need to cobble together the Service Element from the Sysinfo program and the Internet Radio program so that i can get the Pi to start up the generator as a service on start up so that users don't need a console or TTY connection to use it.   I do have some pictures to share, though, as I have been looking at the possibili ...
Application Information http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/04/22/some-information-from-my-application ChipKit Pi Vs Arduino Pro Mini http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/01/quick-update-on-the-quadcop-and-the-chipkit-pi Quadcopter Assembled (You call that a Quadcopter?) http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/06/quadcopter-assembled Quad ...
Introduction Reference docuemtation Meditech NTP client-server architecture NTP Server NTP Bridge client-server NTP Wireless client Common to all devices NTP configurations in practice NTP main server (RPIslave1) NTP bridge client-server NTP client Remember to restart the NTP service Introduction The Meditech architecture is based on a certain number of Raspberry PI (initially three in the actual prototype) every one dedicated to manage specific ta ...
Previous posts for this project: Sci Fi Your Pi: PiDesk - Project Description Sci Fi Your Pi: PiDesk - Project Update #1 Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2 Sci Fi Your Pi: PiDesk - Project Update #2 Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board Sci Fi Your Pi: PiDesk - Project Update #3 Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot Sci Fi Your Pi: PiDesk - Project Update #4 Sci Fi Your Pi: PiDesk - Project Update #5 Sci Fi Your Pi ...
Introduction Software Hardware Demo   Introduction  Addressable LEDs or NeoPixels are typically used in combination with an Arduino or similar microcontroller, due to the timing critical signal required to control them. An SBC such as the Raspberry Pi is not suited for such realtime GPIO activities, as the Linux operating system runs other tasks in parallel. Or at least that was the case until Jeremy Garff found a way to use the DMA (Direct Memory Access) module to tra ...
After a full-discharge the battery used for testing has been recharged with the simple circuit mentioned in the post Powering the camera probe for few hours to test if the charging circuit, experimental and very simple, may have problems .   Test conditions  7,5 Vcc / 1500 mA LiIon rechargeable battery Full charge done (about 3 hours) with the LM350 based battery charger Power regulator based on LM7805 Raspberry PI B+ with camera running continuously with the frame capture program. ...
The ZD1211 choice As mentioned in previous posts, the Camera Probe (that is, the RPIslave2) will include a WiFi connection. To make the board more compact and use a cheap but reliable WiFi connection the choice was the ZD1211. In the Linux environment it is a sort of "standard" as the os firmware and kernel modules to support this device is widely diffused on many linux distributions, especially for the embedded linux devices.   As a matter of fact any kind of WiFi dongle supporting this f ...
Introduction As mentioned in previous posts the device RPIslave2 is equipped with the PI camera to capture still frames imaging diagnostics. This probe should be easily moved outside the Meditech unit; it remain connected to the remaining system via WiFi and should be battery-powered. The powering characteristics should be the following:   When hosted in the Meditech unit the device is powered-up running in stand-by mode: some features will work but it is not possible to manage the camera ...
Introduction An important change in the UI strategy Production costs reduction Data exchange security improvement Qt 5.3 testing Introduction Inside the Meditech architecture the platform RPImaster is the deviced that has the main role of server coordinating the system of probes, storing data, streaming and more. In few word the RPImaster device will assolve the following tasks: Bridging between the internal network and the external internet connection Apache web server wit ...
Prelude My initial design was to build a set of robots around the raspberry Pi and use other components in the kit to build the control systems. Since I am yet to receive the kit, I have moved to researching the Image capture and recognition part of the project.   Introduction OpenCV (Open Source Computer Vision) is a library of programming functions mainly aimed at real-time computer vision, developed by Intel Russia research center in Nizhny Novgorod, and now supported by Willow Garage an ...
The Machine-2-Machine protocol, MQTT, has really forced me to rethink how to organize the whole communication process of this project. MQTT stands for Message Queue Telemetry Transport and is touted as the protocol for the developing world of IoT (Internet of Things). Developed by Andy Stanford-Clark and Arlen Nipper, MQTT has been around since 1999. I heard about it while scouring the Raspberry Pi forum for information on communicating between two Pi's over TCP/IP.   Here's what the offic ...
This is the first preview of the microscope camera that will be one of the probes connectable to the Meditech unit for micro-surface investigation e.g. skin, pariculars and so on. The video shows an example at about 200X magnification. As much the magnification increases, as the DOF is short. The device will be protected in front by a transparent circle and thanks to the internal leds ring light it can be put directly on the subject surface.   Next step: stream the real-time images on ...
Previous posts for this project: Sci Fi Your Pi: PiDesk - Project Description Sci Fi Your Pi: PiDesk - Project Update #1 Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2 Sci Fi Your Pi: PiDesk - Project Update #2 Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board Sci Fi Your Pi: PiDesk - Project Update #3 Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot Sci Fi Your Pi: PiDesk - Project Update #4   Project Update   Project Update  Las ...
IntroductionInstead of using the samba protocol, that is more resource consuming and is needed only when the network files should be shared including Windows machines or other desktops or anyway for some specific needs, a better solution to share folders between several linux machines is through the NFS file system.   Server install and setting Installing the server side on raspian should be take in account a couple of issues that affect this Debian distro. First of all we have two options ...
A component that is very important for my project arrived: the projector! The very generic-looking box Projectors can get really expensive, but as you can see I went with a budget version. For around 50 bucks you can find yourself a Chinese-made projector that does 480x320 and has a brightness of 100 lumen. If you're thinking that's pretty pathetic, I agree. I decided to spend a little extra and got myself one that did 640x480 (at only 80 lumen) for 70 bucks. This way R2-D2's projector would ...
Introduction and usage Setting the capture side startcam.sh stopcam.sh The sharing strategy The still image streaming process The streamer application The streaming command Introduction and usage One of the most versatile probes of Meditech is the camera that cover a meaningful wide range of applications shortly described below   Screening of areas, like skin or injuries detail for post-intervention documentation or to describe particular environmental chara ...
frellwan

FTP Code Working

Posted by frellwan May 11, 2015
I have ordered a USB to RS232 cable (USB-RS232 WE) to be able to communicate to the AB SLC PLC I have ordered a USB to RS422 cable (USB-RS422 WE) to be able to communicate to the Fenner M-Trim controller   FTP Communication While waiting for the above cables to arrive, I have been working to get the FTP communications working        OEE data      Data will be read from the PLC every minute and stored to a local file. The local file will be s ...
Hello   The parts arrived a week ago and I was glad to find all essential pieces inside.   The first step was to check the RaspberryPi_V2 and install Raspbian, 2015-02-16 at that time (I saw a new one - 2015-05-05 - came out since) and made usual configuration, expand FS, enable camera and network configuration for remote access.   This was my first contact with the RaspberryPi_V2 and I'm pleased about it. Improved CPU, Micro-SD slot and the 4 USBs are so far the most importan ...
Application Information http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/04/22/some-information-from-my-application ChipKit Pi Vs Arduino Pro Mini http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/01/quick-update-on-the-quadcop-and-the-chipkit-pi Quadcopter Assembled (You call that a Quadcopter?) http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/06/quadcopter-assembled Quad ...
Previously: Sci Fi Your Pi - Prince Dakkar's patent log taking chart compass       To realise my initial ideas for the project I have started work on designing the functionality of the device.   This really divides into three main function sets; indicating the users current position, setting the route to be navigated and, Indicating the route and direction of travel.   Indicating current position The device will indicate the users position on a map. The position wil ...
dmrobotix

PizzaPi: Quick Update

Posted by dmrobotix May 10, 2015
Hello, everyone!   Sorry I have not posted much recently. I would be remiss in my contestant responsibilities if I did not keep up with my updates and give a quick heads up on how things are going with PizzaPi!   Last week I started my 10-week full-time internship at the lab I work at and its been a bit of a challenge getting used to working all those hours! I'm actually spreading these 10-weeks over a 20-week period, so in a few weeks I'll be off again and I'll be more active around ...
Hello all! Been busy getting everything connected and initialized for the build. Successfully connected Gertbot, MEMS board, and Pi Camera. I've got them successfully communicating through a Pi Rack onto the B+ (as the MEMS refuses to work with the Pi 2). I have noticed that whenever the Gertbot is driving my test motor that the MEMS readings really wig out. Ultimately I think I will have both Pis running in the project - a navigator and a driver. I'll have the B+ connected to the MEMS board, Pi ...
taodude

I Ching Blog Week 2

Posted by taodude May 9, 2015
Finally getting to grips with using Python and the PiFaceCAD and accessing the Pi using SSH/PuTTY. but I'm having less success writing blog posts that have all the fancy formatting that others are using, probably because i am writing the blogs late at night as a summary of the previous day or so's activity.  Also, this Blog engine has not been programmed to autocorrect my dyslexic fingers.   I'm on the road this weekend and most of next week, and i haven't quite go the project to the ...
After probably having broken my pi camera last week, I tried to revive it, but to no avail. At this point it's probably safe to call it a lost cause. I wasn't too worried over it. I have 2 USB webcams lying around and I figured I might be able to just use one of those instead instead. In fact, these USB webcams have a built-in microphone. In absence of the Cirrus Logic audio card, that would really come in handy!   Meet Laurel and Hardy   The left one is a Microsoft LifeCam VX-3000 ...
The software solution to create a bridge in the main device, able to manage the internal network and the external WiFi connection convinced me that this was probably the best solution to deliver all the needed features:   All the Meditech RPI can be accessible logging to the Master RPI via ssh or from the graphical desktop The internal devices can access the Master RPI device via the internal LAN sending their data to the storage database (MySQL based) via http / https and PHP The intern ...
The reason of this documental note is to underline the elements that should be took in account with the project respect the use of some connection strategies, i.e. the adoption of the Bluetooth for printing and - where it is possible - some probes and the WiFi connecting the diagnostic part with the display control.   I tried to keep this document as short as possible argumenting the aspects with some attached PDF and specialised sites links. A general-interest document is Know your regula ...
Introduction Setting up the RPi Python GUI over the local network. On the Remote Machine Grove Pi+ or else Getting started. Enabling I2C and SPI on the RPI I2C tests A Little Tinkering   Introduction  In the last post, I described the hardware part for our robot which uses the Seeed Studios GrovePi+ since I am yet to receive my kit. In this post, I talk about the software part and making the robot move. Lets see what we can do.   Setting up ...
augusto.diniz.l

C-3p1 - update

Posted by augusto.diniz.l May 7, 2015
So, since my kit will take a month to arrive, i'm dealing with the things that i can...   Shelf - well since i can't import one from anywhere (as far i was tempted to that, but taxes here is a robbery - around 100%), i have a buddy here in Brazil that's making those helmets in fiberglass, i'm getting one from him. threepio sound: gathering from my personal collection, and "cleanning" it with adobe audition... on that first stage, i will just add treepio voices in english and potuguese, ...
trenchleton

Kit Content

Posted by trenchleton May 7, 2015
Just wondering - is anyone else still waiting on part of the kit? I haven't received the RPi A+, audio card, Microstack GPS, or Microstack baseboard. Did the kit get changed, does anyone know? Beggars can't be choosers - I was just hoping to utilize a couple of those other parts. ...
Previous Posts   Application Information http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/04/22/some-information-from-my-application ChipKit Pi Vs Arduino Pro Mini http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/01/quick-update-on-the-quadcop-and-the-chipkit-pi Quadcopter Assembled (You call that a Quadcopter?) http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/06/qua ...
Why to avoid other attracting alternatives for the internal boards connection than LAN An alternative, detailed point of view My point of view The most important reason to adopt the Ethernet connection Bridged networking Introduction The networking part has two main roles:   Meditech device internal communication between the specialized RPI units that are part of the system and, optionally other RPI connected as add-on External wireless communication with the display u ...
Mobile unit for on-field interventions The medical tricorder Meditech is a modular specialized version of the standard Starfleet tricorder (it will not be in service on the starships before the 23rh Century). It is equipped with sensors and analysis software tailored for medical diagnostic purposes. These sensors will collect, store and organise data to be used, especially in emergency and crytical situations on the Earth and other exoplanets, when assessing a patient's condition.   The fu ...
Hello all! I am behind everyone else I realize - I will do my best to make up for this in the coming weeks! I'm a full-time student going into finals, so I've been quite busy!   I also thought I'd share another side project which has robbed me of my pi time. I'm involved in the Science Outreach Club at my college. We do hands on activities for students in our (quite rural) area. It gives them the opportunity to experience STEM in a way they might otherwise not have been able. I spearheaded ...
Previous Posts   Application Information http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/04/22/some-information-from-my-application ChipKit Pi Vs Arduino Pro Mini http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/01/quick-update-on-the-quadcop-and-the-chipkit-pi Quadcopter Assembled (You call that a Quadcopter?) http://www.element14.com/community/community/design-challenges/sci-fi-your-pi/blog/2015/05/06/qua ...
Previous posts for this project: Sci Fi Your Pi: PiDesk - Project Description Sci Fi Your Pi: PiDesk - Project Update #1 Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2 Sci Fi Your Pi: PiDesk - Project Update #2 Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board Sci Fi Your Pi: PiDesk - Project Update #3 Sci Fi Your Pi: PiDesk - Guide: Stepper Motors with Gertbot   Project Update   Project Update  Had some fun with stepper motors today! I've be ...
Introduction Setting up Script Demo   Introduction  The Gertbot is an add-on board for the Raspberry Pi, compatible with all existing models.   It brings power and motor control capabilities to the Raspberry Pi, but can also be used with other controllers supporting serial communication. Because the Gertbot has it's own CPU dedicated to the real time activities, the Raspberry Pi is only required to pass high level commands such as "DC motor 1, ON", "Stepper motor ...
View all my posts on this project here: http://www.element14.com/community/tags#/?tags=quadcop_project   Got an update coming on some technical hardware, in the interim,  Got my quadcopter assembled!   The kids wanted to be in a video so here it is, cheesy as it gets.  This is the Quadcopter I will be using for testing of the QuadCOP.  I plan to get something sleeker later in the project.     ...
The early stages of software development often takes time to produce tangible results, particularly when you are climbing the learning curve of several technologies at once with crampons and ice-axes, but no rope .   However, thanks to the documentation provided for the PiFaceCAD Examples — PiFace Control and Display (CAD) 2.0.7 documentation, and the documentation that comes with Python, plus a small injection of brain power by yours truly, we have a first example of the Hexagram Di ...
Introduction The setup procedure Installing the components Pairing and stable connection with the printer Python printing example Introduction The need is to create a reliable and fast, simply to modify command set (as a matter of fact should become a Python library) to control the printer features. The small thermal ESC/POS printer, supports a well known protocol able to generate all the needed printout we need. Adopting a Bluetooth enabled printer has the great advantage t ...
Introductory note In this document I will show the results, in a separate post I will publish the setting procedure.   As mentioned in a previous post, a small thermal printer will change the rules of the game tracking the history of an emergency intervention. In unconventional situations I have personally experienced that it maybe useful that some data are on paper instead of in digital format only. The other point is that some health status reports are better to be printed for a lot of r ...
In the previous post Meditech: Powering the unit  michaelkellett rose the problem of electrical safety and general medical devices compliance about the possible risks adopting some components, especially related to the power supply architecture.   It is clear that as Meditech will be a medical device patient safety from any possible device derived injuries should be considered in depth. The actual phase of the project, that is the definition of the parts and the general architecture, ...
Printer is here!  Well this is the Meditech printer (or what it will become in very few time, hopefully).   Hardware details  Printing method: thermal on paper rolls 5 inches wide (about 55mm) Printing speed: 90 mm / min Power supply: 12V CC Communication: Bluetooth 4.0 Printing protocol: ESC/POS standard protocol (aka EPSON protocol) Monochromatic graphic support   State of the art Next step is to make it printing on the Raspberry PI while for now the RPI has been ...
Powering Meditech As Meditech is almost complex several power levels should be provided. To simplify the scenario the elements that should be powered in the base architecture are listed below   Storage: hard disk(s) will be low power 2.5 inches devices but it is to exclude the adoption of some kind of static SDD due the too high price per gigabyte. Maybe in the future these prices dramatically decrease so this kind of reliable solution become affordable. Processor units (at least two): we ...
frellwan

Ready to start!!

Posted by frellwan May 4, 2015
Received most of the kit parts - really all of the parts that I need for my project.   I need to order the following cables to communicate to peripherals:   USB to RS232 (9 pin Din connector) USB to RS422 with wire end exposed.     So to recap my project:   Today’s manufacturers are looking to continuously improve their processes to be able to increase quality and reduce waste and cost. Part of the continuous improvement initiatives includes Overall Equipmen ...
My Gallery Title PCD8544: Front of PCD8544 LCD Display. Back of Nokia 5110 LCD Display Nokia 5110/3110: Front of LCD Display Speaker Assembly: Component removal Stereo Speakers: With amplifier R2D2: Helper, Butler, and confidante' It has been busy this week, although the blog has taken some time to put together. I've been gathering a few more supplies necessary for the construction of the container for the "Picorder". While that is in progress, I've set in motion some basic te ...
As the RPI master will act as a server and data collector, centered on MySQL database it has been clear from the start that a large storage solution has to be adopted. This can be done in two possible ways:   Adding an external USB hard disk for storage only leaving the entire OS on the SD card Replacing as much as possible the SD card moving the entire RPI OS and storage system on the external HD   Considering the pros and cons, the decision was to find a way to move the entire sys ...
Previous posts for this project: Sci Fi Your Pi: PiDesk - Project Description Sci Fi Your Pi: PiDesk - Project Update #1 Sci Fi Your Pi: PiDesk - Guide: Setting Up the Raspberry Pi 2 Sci Fi Your Pi: PiDesk - Project Update #2 Sci Fi Your Pi: PiDesk - Review: Bare Conductive Touch Board   Project Update   Project Update  Last week I started experimenting with a component which isn't part of the kit. As described in my very first post, I plan to use the Touch Board for ca ...
First key points assuming as definitive More than one Raspberry PI: networking Three main classes of probes 1. Heart and general health sensors 2. Non-invasive internal analisys 3. Glucose analisys Hard-copy low priority tasks It is time to discuss the adopted development strategy for the entire project whose main complexity IMHO is that involved different technologies and need almost different approaches. Especially because the final point it to harmonise all the i ...
Introduction In The Box Setting Up Preconfigured Arduino IDE Hardware Libraries Code Electrodes MP3 Project Conclusion   Introduction  Last year, I backed a project on kickstarter by a company called Bare Conductive: the Touch Board. The Touch Board is an Arduino compatible board, based off the Arduino Leonardo, which adds new features such as: capacitive touch chip MP3 Player LiPo battery charger stereo output microSD slot ON/OFF ...
Hi all,        This post is nothing but some of my thoughts on ideas that I have proposed for this challenge. And it will be short too.        By the way, this week I received KIT from element14, and as like all I got very excited to see and work with them.   I am not going to describe about KIT contents as they are available on element14, and I don't want to duplicate them here. All I am going to give is just a link where you can fi ...
kcrajesh

PiBo - a soft start

Posted by kcrajesh May 1, 2015
I dreamt of using Windows 10 on the Raspberry Pi 2 for my project. There is more to go for this but the possibilities are amazing. Microsoft announced the Windows Core yesterday and have made available a preview download of the core. I was able to get it to boot the RPi 2, write some code on Visual Studio and debug them on the board. The core has still a way to go for completion, but the version they have out is pretty good.   Here is an image showing the default app. The core does not hav ...
Introduction Where to start Making a Chassis Setting up a Raspberry Pi The additional Hardware   Introduction  As described in my previous post, my project has sub modules. Each has a Sci Fi Purpose and it should all come together to complete project VIRUS. OR I may divert all together and do what I see more fun to do. In this post, I start with making a robot. I will try and write these posts out in the form of tutorials so that you at home can follow along. Lets ...
Other posts on my project: http://www.element14.com/community/tags#/?tags=quadcop_project   I am working on a real update for my project.  I have several parts connected up and nearly 1000 lines of C code written for my arduino and my Raspberry Pi2.  I have some things to demonstrate and some explanations to do.   I decided to take a tangent and work with the ChipKit Pi.  I remember a few years back I wanted a Chip Kit UNO because it was a 32 bit processor that is muc ...