Skip navigation

Smarter Life

6 Posts authored by: Kilohercas Top Member
...
Android keyboard emulation on my hardware     This is quite good learning process. I mean, it is simple, but at the same time it is quite complex. Like i can't use coma more than one time, and if i delete it, i can use it again. Simple, but need additional code to make it work. Also cursor jumping, if i push cursor to front, first i have to shift numbers to left, and only when i can write new number, also have to make sure that number size is less than 4 digits, if i try to shift 3 ...
2 days work on exterior and today i can say, it turns out better than i expected . Now only UI programming is left, RTC, PID,PWM are working and i can do reflow soldering even today, but i need to make clean UI. Still don't know how can this project be completely ignored by in this contest, but where is other contest on STM32F429 that needs to explore DMA2D peripheral and what is exactly what i need for my user interface, alpha blending for 2 temperature graphics, also transparency for on scree ...
Quick update   ...
...
Hello, i would like to present my Smart Life challenge idea.   I am thinking about making reflow oven. It will have 3.7 inch capacitive touchscreen with 800x480 AMOLED or SLCD screen for user interace as well as encoder for setting up time and temperatures of each reflow process steps. (maybe i will going to use unipolar stepper for this function, since it has very positive feedback, and very long life span )     PSoC4/5 will run control algorithms for heating, and so on. I will ...