Skip navigation
<< Previous Post Table of Contents Real Time player Monitoring System User Manual Introduction: “Real time player monitoring system” is low cost open source project for measure and notifies vital body parameters of sport person or entire team (i.e. Heart Rate, Body Temperature, Helmet Impact Force and Chest Impact Force) to coach Via WiFi Link. Heart Rate, Body Temperature and Chest Impact Force are sensed by Chest Strap module and Helmet Impact is sensed by helme ...
<< Previous Post Table of Contents Next Post (User Manual) >>   After almost 5 months of hard work with many sleepless nights, finally the day came for final submission for Sudden Impact wearable Design Challenge... before going to my final prototype I would like to start with my initial proposal...   Project Title : Real Time Player Monitoring System   Project proposal: Designing of low cost, easy to use and battery powered wearable sensor module to stream and m ...
<< Previous Post.. Table of Contents Next Post >> With Continuation to my Previous Post.. where I have shared all GUI Related codes and executable application, In this post I am Sharing My Hardware Details and mcu Source codes in open source domain...   1. Hardware Schematics, Hardware Details and PCB Layout   1.1 Schematic of CC3200-MOD based Master mcu Module for Chest Strap:         1.2 Schematic of MSP430 Slave mcu module for Halmet ...
<< Previous Post.. Table of Contents Next Post >> A Promise is Promise...... I have promised that I will release all the content of my project under Creative Commons BY-SA License so other interested people can replicate my work or even contribute to it...   Today, I am releasing all my GUI Design related Work of Real Time Player Monitoring System for open source community...   1. GUI Application: Main features of this Application are, Can monitor entire team ...
<< Previous Post Table of Contents Next Post >> Here is demo video of CC3200-mod based Chest Strap and Halmet mounted wireless impact sensor in action with android App..   This video shows demo of CC3200 -mod based chest strap module working with Android App... I havn't wear this module so even I have interfaced AD8232 Heart Rate monitor, I am sending junk data to app for heart rate.. Temp sensor ADT7320 is interfaced and data are perfect.. ADXL375 Accelerometer is on CC3200-m ...
<< Previous Post Table of Contents Next Post >>   Following picture shows DIY Chest Strap for heart rate monitoring using AD8232 AFE... Here is Short Video Showing Working of MY DIY Chest Strap with AD8232 and Copper clad PCB as ECG Probe to monitor heart rate..   I observed that if area of ECG Probe is increased it gives better results...in future I am planning to design these ECG Probes using conductive fabric https://www.sparkfun.com/products/10070 for get better ...
<< Previous Post Table of Contents Next Post >> In my Previous Post, I have shared my PCB designs and Testing of CC3200MOD based main MCU board..   Today I am sharing my work towards get the final build...   To improve form factor of AD8232 evaluation module I have removed all switches, Connectors and Jumpers and hard wired the module as per my requirements.. Ultimately the thickness of module is reduced so thickness of final wearable stack of all boards will be r ...
<< Previous Post Table of Contents Next Post  >> In my Previous Post ,I have shared testing of android app for realtime player monitoring system with dummy UDP packets over WiFi. I have almost done with PCB design for my Final Prototype... and here is my PCB layouts...         Edited on 14/4/2015.... Initially I am using TI Fuel tank boosterpack with single cell LiPo to power up all sensors and mcu... meanwhile I am also designing LiIo ...
<< Previous Post Table of Contents Next Post >>   Here Is Android App demo for Real Time Player Monitoring System... In this video I have shown testing of my android app for real time player monitoring system... Dummy UDP Packets are sent from PC using Packet sender application... Recorded screen on right side shows demo of my android app.. This app is designed with Processing 2.0b7 and same app can be compiled for Windows/MAC/Linux PC.. I am progressing well in hardware ...
&lt;&lt; Previous Post Table of Contents Next Post &gt;&gt;   In My Previous Post I have shared Impact detection algorithm.. Today I am going to share AD8232 based heart rate monitor demo.. I have just used 4x5cm PCB as ECG Probe and TLV3402 Comperator to detect heart beat and to give interrupt to MCU (cc3200 in my case), Probe Placement is shown in video. AD8232 Switch and jumper Configuration is as below... Here is demo video of AD8232 based heart rate monitor... ...
<< Previous Post Table of Contents Next Post >>   In my Previous post…, I have shared my Initial Android application that supports Realtime graphs of Accelerometer data.. In this post I am sharing Full Proof Impact detection and remote update algorithm..   Here is detailed algorithm..   Step 1 - Sample rate for Raw accelerometer data reading is currently 1000 Samples/second and it can be increased as per requirement up to Maximum ADXL375 Update rate ...
<< Previous Post Table of Contents Next Post >> In my [Previous post I have shared my work regarding interfacing ADT7320 temperature sensor with CC3200 Launchpad using SPI. In this post I am sharing my initial GUI App for Android/PC with Graphing capabilities...Still it is initial version and I have found that coach who monitors vital body parameters of sport person on field, does not need graph but some kind of bar graph with audio visual indication when certain threshold li ...
<< Previous Post Table of Contents Next Post >> In my Previous Post , I have shared interfacing of ADXL375 High g Accelerometer with CC3200 LaunchPad.   In this post, I am sharing Interfacing of ADT7320 Temperature sensor with CC3200 LaunchPad and Body temperature measurement with ADT7320. ADT7320 is High resolution Temperature sensor (Resolution 0.0625°C/LSB in 13bit and 0.0078°C/LSB in 16bit mode). Maximum Temperature measurement range is −20°C to ...
<< Previous Post Table of Contents Next Post >>   In my Previous Post , I have discussed Interfacing TMP006 contact less temperature sensor with CC3200 Launch Pad.... In this week I have received all Kits from ADI as part of this design challenge...   Today, I am sharing interfacing of ADXL375 +-200g Accelerometer with CC3200 LaunchPad, Using the same code you can Interface ADXL375 with Arduino or MSP430.... etc using Arduino or Energia or any uc Supporting Arduino like ...
Real Time Player Monitoring System Table of Contents   Sr No. Link to Blog 1 [real_time_monitor] Real Time Player Monitoring System Post#1 : Introduction 2 [real_time_monitor] Real Time Player Monitoring System Post#2 : Playing with CC3200 for UDP communication 3 [real_time_monitor] Real Time Player Monitoring System Post#3 : Playing with CC3200 for SD Card Interfacing 4 [real_time_monitor] Real Time Player Monitoring System Post#4 : Contact less Body Temperature Measurement using TMP0 ...