Blog List: Garbage Collector #1 IntroductionGarbage Collector #2 Clamp testingGarbage Collector #3 Seeking help from Infineon's Technical SupportsGarbage Collector #4 Some basic interactions with the shieldsGarbage Collector #5 Base testingGarbage Collector #6 Wireless ControllerGarbage Collector #7 Clamp and BaseGarbage Collector #8 Clamp ImprovementGarbage Collector #9 Doubling the maximum currentGarbage Collector #10 Summary With pandemic such as Covid-19 going through all aroun ...
Thunberg received the prize after being the awarded the inaugural Gulbenkian Prize for Humanity. Even when being honored Thunberg gives back to fight against climate change. (Image credit: Michael Campanella/The Guardian) Greta Thunberg is one of the most inspiring figures in recent history. Her actions in the fight against climate change earned her the inaugural Gulbenkian Prize for Humanity, which includes 1 million euros ($1.14 million). Rather than keeping the prize, the 17-year-old ...
We are just extremely lazy. That's my motivation. This mission has very deep roots. It began with me, my flat mate and the garbage truck that comes to our society to collect the garbage every morning. While emptying the dustbins we have to make sure that the dry and wet waste are in separate dustbins. It so happens that, at least a day in a week, I will be out, getting scolded over why there is mixed wet and dry waste. Thanks to my flat mate (or maybe me, I will let you decipher th ...
Thankyou infineon and element14 community e14phil danzima for choosing me one of the official challenger of sustain the world design contest. First blog THE HOME SUPER SMART Eco friendly design of residential apartment buildings with excellent use of home automation. The world have evolved into a global village where pollution, disasters, diseases have spread to a maximum range. In this type of chaos, it is very necessary to preserve the earth and the living things that e ...
Blog Posts .... Blog #1:Measure Climate Change with Hydroponic System Blog #1 | Concept Design and Plans Blog #2:Measure Climate Change with Hydroponic System Blog #2 | XMC4200 Bring-up and Hydroponic System Blog #3:Measure Climate Change with Hydroponic System Blog #3 | XMC4700 + DC Motor Shield with Hydroponic System Motivation Today, people are concerned about global warming and climate change. However, as climate is defined as “ the weather conditions that are expected in a r ...
Concept of the project f we can reduce the food waste from every house. It will reduce the cost of garbage management for the city. And if we can recycle food waste. it’s will improve the environment. This project “ Food waste recycle bin “ will convert waste food into natural organic which we can use to plant the tree. Users just put waste food into the slot for the crusher. Food will be shred into small pieces and the controller ...
Phase ona: My original and ultimate concept is for crop circles that are a square acre each in size. This is really meant to be a self sustaining vocational training program for industrial evolution, with a biproduct that feeds and houses. I So, for my first phase I am going to work on how to create a working scaled down model. I'm going through the options I have been considering as well as the cost due to extremely low budget. In place of a circular canal system being trenched on the a ...