Hi All, In the previous blog7 i have finalized the setup and in this blog I'm going to add Eink display to the XMC4200. The Eink display ( eINK Click board ) i have got from the Mikroe and i'm using the 1.5Inch EPD display. SPI Interface: The EPD is interfaced to our XMC4200 with SPI interface. The board has an Mikroe slots we need to insert the module. Pin Details: #define EPD_RST P2_7
#define CS ...
It has been a long time, in these complicated times of Covid-19. Since my initial project I have changed a few things. The main one was instead of using the Platform2GO XMC4200 I preferred to use the XMC4700 RELAX LITE KIT that has greater support in Arduino and therefore faster to carry out prototypes. In the development I will test the necessary parts separately and then integrate the project. My project is divided into 2 parts. 1.- inside the house where I will monitor da ...