In summer watering plants is must also it is the most difficult time for container plant watering, the amount of water may vary from species to species. Container plants outdoors need more water than those indoors. This is because higher temperatures, direct sunlight and wind, dry the soil quickly. So in early morning or early evening is the optimal time to water the containers, as this will give the plant some time to take up the water. It takes much to water and it is tough time to protect the ...
The hardware is setup to water the plants in different areas to water the plants in different quantities. The video shows the working of the watering System. ...
The software program is important to control the watering system to water the plants in different pots with different water quantity. #include <SPI.h>
const int EN = 8; // Set pin 8 to control Enable pin of TLE94112
const int CSN = 10; ...
Installing the setup to different pots is important and in home the pots will be located at different places like in garden, balcony, hanging, etc. In the present blog I would like to give on idea to set the watering time for different sized pots. In the below figure the two pots can water upto ONE minutes based on Flow Rate 80 L/H. In the below figure Two tray are used for Marie-gold, Zinnia flower plants, roselle plants to grow it require half liter of water that can be distributed with th ...