Blog8# Program to control the Motors to specific time.
Posted by karthickiot in Sustain The World - Design Challenge on Oct 28, 2020 11:35:00 AMThe software program is important to control the watering system to water the plants in different pots with different water quantity.
#include <SPI.h> const int EN = 8; // Set pin 8 to control Enable pin of TLE94112 const int CSN = 10; // Set pin 10 (CSN1) to control CSN of TLE94112 (default) // Addresses of the control registers const byte HB_ACT_1_CTRL = B0000011; // Activation/deactivation of HB1-4 const byte HB_ACT_2_CTRL = B1000011; // Activation/deactivation of HB5-8 const byte HB_ACT_3_CTRL = B0100011; // Activation/deactivation of HB9-12 const byte HB_MODE_1_CTRL = B1100011; // Control mode (PWM enable, PWM channel) of HB1-4 const byte HB_MODE_2_CTRL = B0010011; // Control mode (PWM enable, PWM channel) of HB5-8 const byte HB_MODE_3_CTRL = B1010011; // Control mode (PWM enable, PWM channel) of HB9-12 const byte PWM_CH_FREQ_CTRL = B0110011; // PWM clock frequency and frequency modulation of the oscillator const byte PWM1_DC_CTRL = B1110011; // Duty cycle of PWM Channel 1 const byte PWM2_DC_CTRL = B0001011; // Duty cycle of PWM Channel 2 const byte PWM3_DC_CTRL = B1001011; // Duty cycle of PWM Channel 3 const byte FW_OL_CTRL = B0101011; // LED mode for HS1/2 and active free-wheeling of HB1-6 const byte FW_CTRL = B1101011; // Active free-wheeling of HB7-12 const byte CONFIG_CTRL = B1100111; // Device ID // Address of the status registers const byte SYS_DIAG_1 = B00011011; // Global Status Register const byte SYS_DIAG_2 = B01011011; // Overcurrent HB1-4 const byte SYS_DIAG_3 = B00111011; // Overcurrent HB5-8 const byte SYS_DIAG_4 = B01111011; // Overcurrent HB9-12 const byte SYS_DIAG_5 = B00000111; // Open load HB1-4 const byte SYS_DIAG_6 = B01000111; // Open load HB5-8 const byte SYS_DIAG_7 = B00100111; // Open load HB9-12 const byte WRITE = 0b10000000; // Mask for write commands to control registers const byte CLEAR = 0b10000000; // Mask for clear commands to status registers void setup() { // Setup fo the parameters for SPI communication, set CSN and EN pins as outputs and set EN to High Serial.begin(9600); // sets the baud rate for communication with the computer to 9600 bauds SPI.begin(); // Initializes the SPI bus SPI.setBitOrder(LSBFIRST); // Least significant bit is sent first SPI.setClockDivider(SPI_CLOCK_DIV16); // SPI clock frequency set to 1 MHz SPI.setDataMode(SPI_MODE1); // Set SPI clock polarity and clock phase; CPOL = 0, CPHA = 1 pinMode(CSN, OUTPUT); // sets CSN as output pinMode(EN, OUTPUT); // sets EN as output digitalWrite(EN, HIGH); // TLE94112 set in active mode (ENABLE pin = high) } void loop() { activateMotor1_PWM(); activateMotor2_PWM(); activateMotor3_PWM(); activateMotor4_PWM(); } void activateMotor1_PWM() { writeRegister(HB_MODE_1_CTRL,0b1); // Map HB1 to PWM channel 1 writeRegister(PWM_CH_FREQ_CTRL,0b10); // Set Frequency of PWM channel 1 to 100 Hz writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 % writeRegister(HB_ACT_1_CTRL,0b0110); // Activate HS1/LS2 delay(20000); // Wait 20000 ms writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 % delay(1000); // Wait 2000 ms writeRegister(HB_ACT_1_CTRL,0b0101); // Activate LS1/LS2 delay(300); // Wait 300 ms writeRegister(HB_MODE_1_CTRL,0b0); // HB1 is not mapped to PWM channel 1 } void activateMotor2_PWM() { writeRegister(HB_MODE_1_CTRL,0b1); // Map HB1 to PWM channel 1 writeRegister(PWM_CH_FREQ_CTRL,0b10); // Set Frequency of PWM channel 1 to 100 Hz writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 % writeRegister(HB_ACT_1_CTRL,0b0110); // Activate HS1/LS2 delay(20000); // Wait 20000 ms writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 % delay(1000); // Wait 2000 ms writeRegister(HB_ACT_1_CTRL,0b0101); // Activate LS1/LS2 delay(300); // Wait 300 ms writeRegister(HB_MODE_1_CTRL,0b0); // HB1 is not mapped to PWM channel 1 } void activateMotor3_PWM() { writeRegister(HB_MODE_3_CTRL,0b1); // Map HB1 to PWM channel 3 writeRegister(PWM_CH_FREQ_CTRL,0b10); // Set Frequency of PWM channel 1 to 100 Hz writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 % writeRegister(HB_ACT_3_CTRL,0b0110); // Activate HS1/LS2 delay(20000); // Wait 20000 ms writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 % delay(1000); // Wait 2000 ms writeRegister(HB_ACT_3_CTRL,0b0101); // Activate LS1/LS2 delay(300); // Wait 300 ms writeRegister(HB_MODE_3_CTRL,0b0); // HB1 is not mapped to PWM channel 3 } void activateMotor4_PWM() { writeRegister(HB_MODE_3_CTRL,0b1); // Map HB1 to PWM channel 3 writeRegister(PWM_CH_FREQ_CTRL,0b10); // Set Frequency of PWM channel 1 to 100 Hz writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 % writeRegister(HB_ACT_3_CTRL,0b0110); // Activate HS1/LS2 delay(20000); // Wait 20000 ms writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 % delay(1000); // Wait 2000 ms writeRegister(HB_ACT_3_CTRL,0b0101); // Activate LS1/LS2 delay(300); // Wait 300 ms writeRegister(HB_MODE_3_CTRL,0b0); // HB1 is not mapped to PWM channel 3 } int writeRegister(byte address, byte data) { /* This function sends SPI commands to the address "address" with the data "data" * The data sent by the TLE94112EL to the Arduino Uno (SDO) and the data sent by the Arduino Uno to the TLE94112EL (SDI) are reported in the * Serial Monitor (CTRL + SHIFT + M) */ address = address | WRITE ; digitalWrite(CSN, LOW); // take the CSN pin low to select the chip: byte byte0 = SPI.transfer(address); // send address byte to the TLE94112 and store the received byte to byte 0 byte byte1 = SPI.transfer(data); // send data byte to the TLE94112 and store the received byte to byte 1 digitalWrite(CSN, HIGH); // take the CSN pin high to terminate the SPI frame Serial.println(); // insert a carriage return to the serial monitor Serial.print("SDI:\t"); printByte(address); // write address to the serial monitor printByte(data); // write data to the serial monitor Serial.print("SDO:\t"); printByte(byte0); // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor printByte(byte1); // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor int result = ( ((int)byte0 << 8) | (int)byte1 ); // concatenates byte0 and byte1 in result return (result); } int readRegister(byte address) // This function reads a register and returns the data sent by the TLE94112EL. Data sent and received by the TLE94112EL are displayed on the serial monitor { digitalWrite(CSN, LOW); // take the CSN pin low to select the chip: byte byte0 = SPI.transfer(address); // send Low Byte byte byte1 = SPI.transfer(0); // send High Byte digitalWrite(CSN, HIGH); // take the CSN pin high to de-select the chip: Serial.println(); Serial.print("SDI:\t"); printByte(address); // write address to the serial monitor printByte(0); // write data to the serial monitor Serial.print("SDO:\t"); printByte(byte0); // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor printByte(byte1); // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor int result = ( ((int)byte0 << 8) | (int)byte1 ); // concatenates byte0 and byte1 in result return (result); } int clearRegister(int address) // This function clears a register and returns the data sent by the TLE94112EL. Data sent and received by the TLE94112EL are displayed on the serial monitor { address = address | CLEAR ; digitalWrite(CSN, LOW); // take the CSN pin low to select the chip: byte byte0 = SPI.transfer(address); byte byte1 = SPI.transfer(0); digitalWrite(CSN, HIGH); // take the CSN pin high to de-select the chip: Serial.println(); Serial.print("SDI:\t"); printByte(address); // write address to the serial monitor printByte(0); // write data to the serial monitor Serial.print("SDO:\t"); printByte(byte0); // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor printByte(byte1); // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor int result = ( ((int)byte0 << 0) | (int)byte1 ); // concatenates byte0 and byte1 in result return (result); } void printByte(byte printByte) // This function writes to the serial monitor the value of the byte printByte in binary form { for (int i = 7; i >= 0; i--) { Serial.print(bitRead(printByte, i)); } Serial.print("\t"); }
Comments