Skip navigation
1. Slow Progress 2. The Failure 3. Thing to learn and way to go 1. Slow Progress It has been several weeks with little progress. Study the datasheet of XMC4400 and XMC4200 , even XMC4700. To find out that hidden features of  XMC series. XMC4 series MCU are especially good for motor control and industrial application. The advanced CCU4 and CCU8 blocks can not be found in other MCUs. While PWM function is still available for simple tasks, as of LRPWM. The embedded CCU4/CCU8 b ...
1. What to do 2. How to do 3. Demo 4. Next to do 1. What to do It is fairly easy to use XMC4700Relax kit in arduino, but with XMC4200 Platform2GO. One can not help trying to use it in arduino as well. The official board packages skip XMC4200 Platform2GO, only XMC4400 Platform2GO is available. That is what I am going to do . It takes 3 weeks to go with slow progress , it works and not so difficult. 2. How to do 2.1 First, check the datasheet of XMC4400 and XMC4200, only two diff ...
1 Use Smart Switch and TLE94112 for Arduino together 2 How to use Smart Switch library 3 How to use TLE94112 library 4 Revise on the library and Arrange Pin layout for new project 1 Use Smart Switch and TLE94112 for Arduino together It is great to Use Smart Switch and TLE94112 for Arduino alone, but use them together? At least pins are defined different and can not work together. And the pinout for each board is predefined, if only one Master Host shall be used. All the pins sh ...
1.  Description of Motor Controller  TLE94112 for Arduino 2. Understand TLE94112EL 3. Control with Arduino 4. Next Step 1.  Description of Motor Controller  TLE94112 for Arduino The DC motor control shield for Arduino is equipped with the TLE94112EL, a twelve-fold half-bridge driver with integrated power stages.   Key rating , Brushed DC Motor Control up to 0.9 A peak, 5.5 – 18 V normal operating input voltage, 18 – 20 V extended operatin ...
1. About Profet+2 12v Shield for Arduino Shield 2. Use the PROFET™+12 3. Arduino Library for Profet+2 and Basic Arduino Sketch for Profet+2 4.  Next to do. 1. About Profet+2 12v Shield for Arduino Shield The PROFET™ +2 Arduino Shield with BTS700x-1EPP  can be controlled with general logic IO-Ports of a microcontroller. Either an Arduino Uno R3, the Arduino Due, the XMC™ 1100 Boot Kit or the more powerful XMC™ 4700 Relax Kit and XMC™ 4800 ...
1. The XMC series by Infineon 2. XMC for Arduino 3. KIT_XMC47_RELAX_LITE 4. Platform2GO XMC4200 MCU 5. Design with Arduino 1. The XMC series by Infineon XMC is one of core MCU line by Infineon, this is for general purpose and others for automobile and TLE series for IGBT control. ARM-M0 and Arm-M4 core are covered. As follows, All XMC4000 devices are powered by ARM® Cortex®-M4 with a built-in DSP instruction set. The Single Precision Floating Point Unit, Direct ...
1. The Cooling Peltier 2. Thermal Energy Harvesting 3. How to use 1. The Cooling Peltier Here is the picture , with nameplate rating 12V The principle is simple, as the following picture shows, I have just fetch the pic from other web directly, so, just for reference. It would be better I draw by hand and use my version. The Cooling  Peltier can be heating pad if change side but it is fragile and easy to be damaged when overheating. It is covered with ceramic, so, insta ...
Quick start and copy my application here. I would like to use as many as interesting Infineon Part in this project. Smart Freezer   1. Introduction Smart Portable Freezer is portable and can be used for Medicine distribution like Vaccine or Insulinum. The batterys is included in the freezer to provide power source of 12V, just enough to drive the NPN cooling pad. peltier.   2. Function Blocks 2.1 Battery management Control the battery charging and discharge, record the battery capacit ...