In summer watering plants is must also it is the most difficult time for container plant watering, the amount of water may vary from species to species. Container plants outdoors need more water than those indoors. This is because higher temperatures, direct sunlight and wind, dry the soil quickly. So in early morning or early evening is the optimal time to water the containers, as this will give the plant some time to take up the water. It takes much to water and it is tough time to protect the ...
The hardware is setup to water the plants in different areas to water the plants in different quantities. The video shows the working of the watering System. ...
The software program is important to control the watering system to water the plants in different pots with different water quantity. #include <SPI.h>
const int EN = 8; // Set pin 8 to control Enable pin of TLE94112
const int CSN = 10; ...
Installing the setup to different pots is important and in home the pots will be located at different places like in garden, balcony, hanging, etc. In the present blog I would like to give on idea to set the watering time for different sized pots. In the below figure the two pots can water upto ONE minutes based on Flow Rate 80 L/H. In the below figure Two tray are used for Marie-gold, Zinnia flower plants, roselle plants to grow it require half liter of water that can be distributed with th ...
The power supply for the motor is driven by the TLE94112 Motor driver shield and the regulated power from the source is connected for the GND and Vcc pins in the shield as shown in the below figures. Water Motors are connected to the half-bridge OUT put on the TLE94112 shield as shown in below figure. In the present project four DC water motors are connected. The final interfacing of the hardware are shown in the below figure once the Relax Lite kit is programmed as the appli ...
The below images shows step-by-step to configure and program in DAVE IDE. Program: #include <xmc_gpio.h>
#define TICKS_PER_SECOND 1000
#define TICKS_WAIT 100
#define LED1 P0_1
void SysTick_Handler(void)
{
static uint32_t ticks = 0;
ticks++;
if (ticks == TICKS_WAIT)
{
XMC_GPIO_ToggleOutput(LED1);
ticks = 0;
}
}
int main(void)
{
XMC_GPIO_CONFIG_t config;
confi ...
The arduino Sketch to program to Toggle on-board LEDs on XMC 4700 Relax kit. C program toggle leds in every one second /* Simple LED library flashes on board LED Every second
Simple RTC for Infineon XMC boards with RTC
Demonstrates the use of the LED library
Works with any XMC board that has TWO LEDs on board
*/
/* For on board LEDs */
#include <LED.h>
/* Create an LED object */
LED Led;
void setup( )
{
Led.Add( LED1 ); & ...
Managing the XMC Infineon boards in the Arduino IDE are shown in step by step and examples codes are available in the following URL https://github.com/Infineon/XMC-for-Arduino DC-Motor-Control-TLE94112EL library from the Github URL https://github.com/Infineon/DC-Motor-Control-TLE94112EL DPS368 Barometric Pressure Sensor library from the Github URL https://github.com/Infineon/DPS368-Library-Arduino PROFET-2-12V-Arduino-Shield library from the Github URL https://github.com ...
The software can be used in the project can be ARDUINO or DAVE IDE. Current version of DAVE IDE can be downloaded from the URL https://infineoncommunity.com/dave-download_ID645 and step by step installation was explained in below video you may install the latest version. The Arduino IDE latest software can be downloaded from the URL https://www.arduino.cc/en/Main/Software . Step by Step installation are documented in the following URL https://www.arduino.cc/en/Guide/Windows. ...
In the Present Projects the Infineon Hardware are used to design the "Smart Garden Plants watering IoT System". The below figure are the challenge kit awarded to design the project. MCU Platform2GO XMC4200 has salient features like Arm Cortex M4, 256 kB Flash Memory, 2x Shield2Go Connectors, 1x micro bus connector, Arduino Compatible Connectors, CAN connectivity it is used as a main MCU to control the 6/12V DC motors in Unidirectional and Bidirectional via TLE94112 DC Motor Con ...