Skip navigation
1 2 3 4 Previous

Vertical Farming

53 Posts authored by: m.ratcliffe
Well Im back to making things and have a day a week to work on open source projects just for the fun of it [mainly farming tools], these are mechanical devices but electronics ones will soon follow   As usual the designs are open source, link is below. You will need a Laser cutter. BOM in the thingiverse files.     Want to Make one: https://www.thingiverse.com/thing:3911941     Want to Buy one: Contact mike@aquaponicslab.org Depending on the size of tray you wan ...
Well Im back to making things, I have changed jobs and now have a day a week to work on open source projects just for the fun of it. Seeding takes time and is relatively boring, this dibble plate will mean I have more time to do fun things: As usual the designs are open source, link is below. You will need a 3D printer and Laser cutter. Want to Make one: https://www.thingiverse.com/thing:3866898     Want to Buy one: Contact mike@aquaponicslab.org Depending on the size of ...
Ive been working on some educational material for teaching, Here are the Results.   This is not one of my usual hacking Posts but I think it is a good example of how the hacking tool-set [rapid prototyping] can be used to bring better projects into the classroom. We use these info-graphics to teach about the mechanisms in aquaponics and bring the class into a FabLab to laser cut for themselves and add school Logo's etc. That has got to be more fun than a text book?     As alwa ...
Today is a good day, The introduction of the 3rd Generation Pi is available! I cant wait to see what this does for the loop times of my vision based work on the pi.   See the main page for other information: Automated Green House Blog's Home Page   Intro Its a great reason to continue my work on the fish feeder. In summary the feeder is a relatively advanced demand based fish feeder prototype. [We will be refining this over the next few blogs] The Benefits of Demand based fish fee ...
This will not be a very useful tip for 99% of your arduino projects, but if you are wanting to keep your code running as quick as possible without reverting to C its a handy tip to have.   Ive got a few arduino projects going now where I need to keep my main loops running fast, This is a test to verify that a multiple IF statement finished if the primary statement is false.   In example...  if(A= =false && B== true)  the arduino will move onto the next line of cod ...
A Updated PH Probe, Now gives A Readout For Probe Life and a time alarm for when to Calibrate.   DFRobot were nice enough to send me one of their pH pro MCU probes [Longer lasting] but this tutorial and code will work for any analog pH MCU meter [ebay special etc] these are coming down in price rapidly but I recommend calibrating often.   The Analog pH breakout boards often have a little pot for adjusting during calibration, this is a pain in the ass at calibration time. This new cod ...
Here is a little Video comparing the growth of Hydroponics,Aquaponics and soil in low light conditions.   the Light intensity here in the north of the uk during winter is so low that the plants grow at a very slow pace, it is interesting to see that hydroponics offers very little gain in growth under low light conditions.         Main Blog home Page: Automated Green House Blog's Home Page ...
In Aquaponics systems pH probes fail quickly, it is my belief that this is due to the probe membrane becoming blocked [just my theory, no proof to back it up]. If this is indeed the problem it stands to reason that we could extend the probe life by cleaning the probe during the monthly calibration.   There are two main ways to clean the glass probe: >Mechanically >Chemically  [See link below for selecting the correct chemical for your probe use] http://reagecon.com/pdf/tech ...
Below is a breakdown and summary of the competition entry Adapted_Greenhouse.   So the competition is coming to an end, quite a sad day because this competition has become part of daily life. I would like to thank Element14, in particular Dave for his time and the time of any other un-named organisers, the sponsors [Silicone Labs and Wurth ElekTronik] for investing in this competition. Charles Gantt  also deserves a mention for his summary of the competition on a weekly basis, his sum ...
The Association of Vertical Farming [AVF]: Everyone in the competition has been lucky enough to receive some great products to get their grow under way will know a little bit about who the AVF are but for those of you on the blog but not in the competition, take a look at the website:   https://vertical-farming.net/   The AVF and Element14 have no doubt been working closely together,but the AVF have not been as active in the competition blogs/write-ups as I had been expecting.Howev ...
This competition has been mainly the bloging about systems I already had implemented after some fine tuning,  recently I found a relatively large group of collaborators around 30 miles from my home who have been working on open sourcing aquaponics control systems, small world! Between us we now have access to multiple test systems, high tech work shops and a wide range of skills. Hopefully this collaboration will lead to more efficient, easier to make automated aquaponics systems, cheap ope ...
One of the other collaborators from the aquaponics lab has recently started to build his own system, here is a time lapse of it under construction:     We have learned a lot from building the "FAO  recommended" aquaponics system and  plan on releasing a quicker easier method for those of you who want results fast. ...
So the seedlings have grown to a stage that they are ready for transplanting from the propagator to the aquaponics, hydroponics and soil systems.     Germinated/planted :      20/10/2015 Transplanted:                 24/11/2015     They have grown slow [very slow], this is an expected problem in England during November where the light intensity has dropped consider ...
DFRobot were nice enough to send me one of their pH pro MCU probes [Longer lasting] but this tutorial and code will work for any analog pH MCU meter [ebay special etc] these are coming down in price rapidly but I recommend calibrating often. I'm hoping the pro model can go longer between calibrations and still hold true. I put the probe in some pH4 buffer solution over night and the LCD printout gave a   min:3.92   max:4.02   this was probably caused by a temperatur ...
The Previose blogs  showed how to log data in seperate ways.   Blog:18.1 - On-line Data Logging [data.sparkfun]  Blog:18.2 - Data Logging: SD Card  Blog:18.3 - On line data Viewer [arduino, Ethernet]  It will be useful to have all three methods implemented on the same board, this is a bit tricky because we need to power up the sd card to load data, then configure the data.sparkfun push the data and leave the web_server script running until the next sd and sparkfun log. ...