Skip navigation
DARPA’s LUKE APAS bionic arm features 10-powered degrees of movement and can be controlled using multiple input devices. (via DARPA)   According to an article from the Washington Times back in December of 2014, more than 50,000 troops have been wounded since the War on Terror began. Of those wounded, 2.6% have lost a major limb due in most part to IEDs. So many in fact, that a host of medical and robotics institutions have been designing bionic limbs shortly after the start of the wa ...
Vishal Aditya

17 DOF Humanoid

Posted by Vishal Aditya Dec 28, 2016
ObjectiveThe objective of this project is to focus in R&D ofAI & Machine Learning BriefThis robot is a professional small humanoid robot consist of full aluminum parts, smooth surface with smooth edges not hurting hands, the metal is unbleached, beautiful and durable. The High Torque Standard Servo Motor with Dual Ball Bearing and Metal Gears. Provides 14kg/cm at 4.8V and 16kg/cm at 6V. Replacement for HS-645MG. Arduino Uno R3 based USB 18 Servo Controller is ideal for making Autonomous ...
The robot, METHOD-1, was built by Korea Future Technology and former Starcraft artist Burlgarov. This isn’t a scene from a movie. This is a robot built by a South Korean company. (via Korea Future Technology)   It’s no surprise to see robots that can walk, talk, or do just about anything thanks to the popularity of the robotics field. But this latest robot built by a South Korean company is something you think would only be seen in a video game. And that’s exactly where ...

Filter Blog