Skip navigation
Introduction The NVIDIA Jetson Nano is a compact board approximately 70x45mm in size, with a large heatsink : ) It's got a very powerful microchip, the NVIDIA Tegra X1, which contains four ARM applications processor cores, as well as 128 graphics processing units (GPU). GPUs are used for more than graphics purposes, because it turns out that some of the interesting applications for computers today, to do with neural networks, which can be used to recognise patterns with ever increasing accuracy, ...

Filter Blog