Skip navigation

Single-Board Computers

3 Posts authored by: mconners Top Member
mconners

Odroid C0

Posted by mconners Top Member Feb 25, 2016
I recently picked up one of these sweet little boards, and I have to say I'm pretty pleased. It is a stripped down version of the Odroid C1+, designed to be lighter, and more configurable to suit your end purpose. It is based on a quad core Amlogic S805 running at 1.5 GHz. It sports 1GB of RAM and both micro SD and emmc slots for storage. Oh, and did I mention it only costs $25. I have to give credit to the folks at ameridroid. I ordered this on a Wednesday night, and it was in my mailbox the f ...
mconners

ADC on the Odroid

Posted by mconners Top Member Dec 23, 2014
One of the biggest features that the ODROID-C1 (odroid, from now on) has that is different than the Raspberry Pi B+ is the ADC. This is a welcome addition and will allow you to interface with analog sensors in a very simple way.   I figured I would use a photocell since I just finished doing a photocell blog project for the B+, so everything was in place.   The first thing I did was log into my odroid, and from my home directory type the following commands:   git clone https:// ...
mconners

ODroid - Oh Boy!

Posted by mconners Top Member Dec 22, 2014
I recently picked up one of these little ODROID C1 development boards and i have to say I couldn't be happier!   It's a Quad Core ARM dev board based on the Amlogic S805 Cortex A5 processor with a Dual Core Mali 450 GPU. It comes with 1 GB of RAM and can can boot from 2 sources eMMC and Micro SD. $36.95 US.   It's layout looks very similar to the Raspberry Pi+, and it is almost the same size. Here is a picture of the 2 side by side:     Some of the features: 4 USB Host ...

Filter Blog

By date: By tag: