Skip navigation
I have a Beagebone Black I/O cape on Kickstarter.     Features List Here's the specific list of features that the card supports:   (19) GPIOs GVS pins (3) UARTs GVTxRx pins (1) I2C bus GVSdaSck (8) Channels of 3.3V to 5V level translators Use female to female jumpers to route the GPIO lines to the translator channels 5V side has GVS pins (7) 1.8V analog GVS connections with analog voltage/ground Buffer opamps on the analog inputs 5V pins are all ESD protected pins ...

Filter Blog

By date: By tag: