Skip navigation

BeagleBoard

3 Posts authored by: Jan Cumps Top Member
How to develop a Linux binary for the BeagleBone (any colour) on Windows in CCS, using BB guru Derek Molloy's GPIO lib. This blog has a history. I was working with my very good friend martinvalencia to get this working. This blog shows the end result: how we got it working. Not shown: all our failures when discussing this over Hangouts.   Derek Molloy is arguably the best source for BB tutorials. His libraries are well designed too. Here's an instruciblo on how to use his GPIO lib wit ...
How to develop a Linux binary for the BeagleBone (any colour) on Windows in CCS, auto-deploy it to the BB and remotely debug. No hardware debugger needed - all runs over TCP/IP The great PRU blog from Fred27 inspired me to pick up the BeagleBone Green again. Because he uses CCS as development environment, it makes sense to also use CCS for Linux native C and C++ development.   I've blogged before on  how to set up a BeagleBone C/C++ environment with the ARM DS-5 suite. Both DS-5 ...
This week's embedded.fm episode features Jason of BB:   110: Happiness Is a Warm Puppy — Embedded ...

Filter Blog

By date: By tag: