Skip navigation

BeagleBoard

6 Posts authored by: ninjatrent
Test Driving the BeagleBone Blue RTV The BeagleBone Blue Road Test Vehicle. This test vehicle is powered by the BeagleBone Blue and was constructed from lightweight and cost effective recycled materials. The BeagleBone Blue is ready to go. https://beagleboard.org/blue   Available at http://www.newark.com/beagleboard/bbone-blue/beaglebone-blue-robotics-platform/dp/95Y0640?st=beaglebone%20blue   What is BeagleBone Blue?   BeagleBone Blue is a complete, Linux-enabled robotics ...
BeagleBone Blue - Drive Motor and Steering Servo Tests   The BeagleBone Blue is ready to go. https://beagleboard.org/blue   Available at http://www.newark.com/beagleboard/bbone-blue/beaglebone-blue-robotics-platform/dp/95Y0640?st=beaglebone%20blue Front View of the BB Blue RTV (Road Test Vehicle) Side View Rear View Top View. Bottom View. The motor is powered directly from the BB Blue via 2-Pin JST-ZH Connector. The cable for the steering servo is also conn ...
Here I am testing the operation of micro servos with the BB Blue under  the power of a 1600mah Lipo battery.   ...
Beaglebone Blue Road Test Vehicle   Hello Beaglebone fans! Thanks for stopping by this post.   I am currently test driving the Beaglebone Blue for the Element 14 Beaglebone Blue Robotics Controller Road Test. What better way to test the BB Blue then to build a test vehicle.   This test vehicle is constructed from recycled materials. It is still under construction. Here are some photos of the progress.   The steering servo has not been installed and the motor is not ...
    This is a simple test of the Beaglebone Blue Robotics Controller with a Pan/Tilt Camera Mount. The micro servos that came with the Pan/Tilt are not that great for precision control but will suffice for the purpose of this test. These servos will likely be replaced with higher grade servos at a later time.   I would also like to mention, the BB Blue is being powered by a 12V 2.5A Power Supply. The BB Blue is meant to be powered by a Li-Ion Battery. The battery should arrive ...
BeagleBone Black Wireless in an Altoids Mint Tin   Curiously Stong Mints? No, but it is quite powerful. It's a BeagleBone Black Wireless!!! The Adafruit Proto Cape Kit fits with lid fully closed. In order to accommodate additional components such as sensors, wiring, and others things, it will be necessary to find some Nylon Polyamide Standoffs that are shorter than the 3/16" standoffs used in the photos. These are the standoffs that came with the Adafruit BeagleBone Proto Plate ...

Filter Blog

By date: By tag: