Skip navigation
1 2 3 Previous

BeagleBoard

142 posts
I have got the BB Black for a while but never got time to get started. It is different from Raspberry Pi in some sense. The thing which I liked is that it can boot from an onboard emmc memory chip. This means you do not need to install OS on fragile SD cards. It comes with the installed OS when purchased. So, just plugging it via the USB cable supplied with it will start the boot process.   The default username and password is the following   username:debian password:temppwd  ...
Introduction One of the most powerful features of the BeagleBone Black is the Linux operating system running on it. This can be demonstrated by using both a kernel driver for a sensor and the utilities provided in the Debian distribution of Linux, in this case to make temperature measurements at regular intervals without user invention. For me this was also an exercise to learn more about the Device Tree and the overlays used to reconfigure and add devices. For this example a LM75 temperature se ...
Summary The Adafruit Proto Plate was tested out both as a prototyping platform and as a home for the BeagleBone Black. Its rubber feet made it stay in place while still having a couple of cables hanging from it and the clever cutouts made it easy to plug things in and out. The LM75 temperature sensor is used as a short demonstration of how nice the BeagleBone is with its full Linux operating system. All in all this is a nice way to keep ongoing projects on your desk while still being able to mov ...
Static test of the BeagleBone Blue Ardupilot quadcopter. Warning!! DO NOT OPERATE A DRONE INDOORS WITH THE PROPELLERS INSTALLED!! Even with the quadcopter secured to the bench, it is VERY DANGEROUS to operate inside with the propellers installed. ...
This is a test of the motors on a BeagleBone Blue Ardupilot Quadcopter using a Frsky Taranis QX7 transmitter and the Mission Planner app. ...
Intro As a follow-up to my previous post: Finding Pulsars on Raspberry Pi (BOINC & einstein@home) I also wanted to run BOINC and einstein@home on my Beaglebone Black (BBB).  BOINC is, of course, the Berkeley Open Infrastructure for Network Computing, a crowdsourcing computer clustering system to solve scientific problems.  I have a few BBB setting in a drawer (more than I like to admit), so why not put them to use?  Beaglebone is running a fairly modern debian image, so it ...
Since it was first coined in the 1950s, artificial intelligence (AI) and Machine Learning (ML) have colonized a substantial share of advanced machines. This happened as AI computing, specifically ML, enables a better quality of life with the technology branching into both homes (personal assistant robots) and transportation (self-driven vehicles), and even into persuasive advertising (image-recognition). The list of AI applications seems infinite, bolstered by smarter, more accessible, and more ...
OK, it shouldn't be a surprise to anyone that this board gets H-O-T. It's not something to be held in the palm of your hand, so it's not that critical. Until it is. Because, as all/most CPUs, it halts when reaching a certain temperature in order to prevent a complete meltdown. In its case, its probably around 85-100 degrees Celsius.(I'll update the exact figure if I find it in the documentation)   So one of the key things for maximizing the use of this SBC is cooling it properly. There is ...
BeagleBone Blue For Quadcopter Flight Control The BeagleBone Blue is a Single Board Computer / Robotics Controller created by BeagleBoard.org. https://beagleboard.org/blue     Previous blog posts related to the BeagleBone Blue   BeagleBone Blue Robotics Controller Kit - Linux - Review Test Driving the BeagleBone Blue RTV BeagleBone Blue Pan Tilt Servo Test Beaglebone Blue Road Test Vehicle BB Blue Pan Tilt Servo Lipo Battery Test BeagleBone Blue - Drive Motor and Stee ...
Could anyone give me a quick pointer as to where to look for information on how to transfer a C programme to the BeagleBone AI and then compile it and run it?   I have a C programme compiled in Microsoft that I wish to transfer to a BeagleBone AI. I have had a quick look online and Element14 and so far I have not found any information about this. I am not a Linux user so this may be easy and obvious but when you don't know something it always seems hard. The C programme implements an Artif ...
Introduction Heatsinking Adding a Fan Serial Console Cable Power Supply Powering Up Upgrading the Software Measuring the Temperature Changing Passwords and Adding Users Configuring WiFi Summary   Introduction I was really happy to recently receive a BeagleBone AI single board computer (SBC) from Element14. It's going to be used for attaching a camera eventually! The Gigabit Ethernet interface and high performance should be handy for that. There's ...
Some photos of the BB-AI! Transparent background, for copying into documents:       Some higher-res photos (normal background):         BB-AI dimensions (note - these dimensions were partially measured, so there may be an inaccuracy of perhaps 0.5 mm in places (and maybe up to 1mm inaccuracy in the heatsink position). If there are any errors, please let me know and I'll correct the diagram). The board is 1.6mm thick, the Ethernet socket is ...
I'm testing the CAN peripheral on a BeagleBone. I'll be using my homemade generic CAN driver to implement the physical layer and Thomas Wedemeyer's BB specific instructions. The other device on the CAN BUS, playing the communication partner role, is a Microchip CAN BUS Analyser.   Like most microcontrollers that have a CAN peripheral on board, the Sitara on the BeagleBone doesn't have a physical bus driver. That's something that needs to be implemented separately. The CAN driver brea ...
I'm trying here is to let the real-time units of the BeagleBone generate the signals for a stepper motor. In chapters 1 to 5, I developed PRU firmware that works for 1 stepper motor   In part 6, I switch to a timer controlled version, that should allow for more motors and smoother start and end. Here in post 6a: refactoring the code a first time to extract motor dependent logic from the main loop:   Prepare for More Motors and Motor State  I created the shell for a structur ...
Introduction The PocketBeagle single board computer (SBC) is really tiny. Apart from the size, there are lots of similarities with the larger BeagleBone Black, and there are also some differences.   In terms of performance, it is identical. It has the same amount of memory, and runs using the same processor and the same Linux image too!   To get the size down, it is of course missing many connectors but a lot of functionality within the main chip is brought out onto the two 36-way ...

Filter Blog

By date: By tag: