Skip navigation
In previous blog posts, I've showed how to use small LCD displays as a Linux framebuffer on the BeagleBone Black thanks to the fbtft drivers: BeagleBone Black LCDs with Prebuilt FBTFT drivers BeagleBone Black: build fbtft drivers for latest Linux 3.8 kernel Build fbtft drivers for TI Linux 4.1 kernel   In this post, I will show how to use fbtft drivers on BBB with the latest version of the Linux kernel.  In this case, that is Linux 4.4. Full transcript in this GitHub Gist.   & ...
There's a free online course that walks you step-by-step on how to setup the BBB and get started with embedded Linux development. Also, there are some sample application tutorials in the lectures for gathering weather information, capturing images from a USB camera and streaming them over WiFi and gaining complete orientation (yaw, pitch, roll) knowledge on the BBB platform in real-time streaming over WiFi.   Checkout the course curriculum and enrollment page here:- Developing with the B ...
Texas Instruments has their own Linux kernel repo with branches to support their processors such as the Sitara AM3358 in the BeagleBone Black:   Gitorious@TI: ti-linux-kernel This repo contains a Linux kernel that has been integrated with outstanding TI open source patches based on the open source Linux kernel found at kernel.org Here is a good presentation for TI TechDay 2015 on how TI handles Linux engineering.   The most excellent Robert C. Nelson has m ...
My previous post showed how to use small TFT LCDs as a Linux framebuffer on a BeagleBone Black:   BeagleBone Black LCDs with Prebuilt FBTFT drivers   I showed how to use pre-built fbtft kernel modules to provide the necessary Linux device driver.  However, what if you want to use fbtft modules with a newer version of the Linux kernel?   The BeagleBone Black currently ships with a Linux 3.8 kernel built from Robert C. Nelson's am33x-v3.8 branch.  I do also have fbtft wo ...
BeagleBone Black using Prebuilt FBTFT drivers Debian Image: bone-debian-7.5-2014-05-14-2gb Kernel: Linux 3.8.13-bone50 Drivers: fbtft-2014-02-07-3.8.13-bone50.tar.gz Displays that I used: Adafruit 1.8" TFT LCD (using fb_st7735r driver) Adafruit 2.2" TFT LCD (using fb_ili9340 driver) Photos of wiring and LCD demo Videos of LCD demo Based on instructions from fbtft wiki GitHub Gist with complete transcript of running the below instructions     Step 1: Download, Flash &a ...
My Tor relay running on a BeagleBone Black is even faster after upgrading to Debian 8 (Jessie) and TorProject.org tor 0.2.6 package for Jessie: Thanks to Alison Macrina of the Library Freedom Project for the motivation to upgrade after watching her inspiring talk during the Aaron Swartz's Day 2015 celebration at Internet Archive last weekend:   A quick aside, if you've not seen this documentary about Aaron's life, then please be sure to watch it: The Internet's Own Boy: The Stor ...

Filter Blog

By date: By tag: