• kernel degrade BB-AI

    I have kernel version 4.14.108-ti-r136. when I run clinfo command it gives error: CMEM Error: init: major version mismatch between interface and driver. CMEM Error:     needs driver version 0x4...
    Profile Photo
    created by prathamesh12
  • Beaglebone black wanted to use i2c with c on LCD2004 pcf8574t

    I m new in c programing language and embedded .   i've tried to take some exemples from internet and make them run for me trying to display something.The first i come across this : that use iobb.h . i've tried...
    Profile Photo
    last modified by olty
  • BEAGLE BONE AI FAN CAPE

    Hello   We have one product in that we have used Beagle bone black wireless and it was work well. After that we  thought replace Beagle bone black wireless with beagle bone AI with our existing design. ...
    Profile Photo
    last modified by hareshp
  • SSID and Password change for default access point

    Beagle Bone AI board creates wi fi access point with bootup. Default ssid is BeagleBone-XXXX and password is BeagleBone. Can we change both of them? Is there any way to do it?
    Profile Photo
    last modified by prathamesh12
  • BeagleBone: Build and Debug a Linux C++ Program with Code Composer Studio

    How to develop a Linux binary for the BeagleBone (any colour) on Windows in CCS, auto-deploy it to the BB and remotely debug. No hardware debugger needed - all runs over TCP/IP The great PRU blog from Fred27 inspir...
    Profile Photo
    last modified by Jan Cumps
  • eMMC Flash Storage and microSD Card Boot on BeagleBone

    Hi BeagleBoard Community,   I have a few questions with regards to the boot sequence of the BeagleBone Black Wireless and BeagleBone Blue.   By default, Does the BeagleBone boot from the eMMC flash or from...
    Profile Photo
    last modified by ninjatrent
  • Enabling DCAN0 (Disabling I2C2)

    I'm trying to get DCAN0 to work on the Beaglebone Black (the element14 industrial version). Not surprisingly configure-pin doesn't work out of the box since I2C2 is used for Capes.   root@beaglebone:~# config-pi...
    Profile Photo
    last modified by robert1
  • New Beaglebone Green Model, "BBGG"

    I had not seen this model before: Seeed Studio Beaglebone Green "Gateway" model. https://www.seeedstudio.com/SeeedStudio-BeagleBone-Green-Gateway-p-4586.html   It is surprising to see a new model of the beagle...
    Profile Photo
    last modified by mp2100
  • BeagleBone Rover Might Be Dead.

    My BeagleBone Black Wireless has stopped working.   When the BeagleBone with Robotics Cape is powered, all the LEDs on both the BB and Cape are blinking once every second.   I suspect that it might be a pr...
    Profile Photo
    last modified by ninjatrent
  • BeagleBone® AI Fan Cape

    The BeagleBone® AI Fan Cape is a simple add-on cape with pass-through pins on the BeagleBone® headers. Once attached, the fan cape will keep the BeagleBone® cool, allowing it to run at the maximum 1.5Gh...
    Profile Photo
    last modified by Christopher Stanton
  • BBB's serial port is not receiving any data.

    Hello,   I have a problem in my BBB(BeagleBone Black) board.   I received BBB today. So I tried to test. First of all, I checked serial port for debug. I could see boot logs with putty. However, I could ...
    Profile Photo
    last modified by jmseo153
  • Beagle bone Black Window 10 Driver Fix

    After receiving my first beaglebone black a couple of weeks ago, I was eager to get started playing around with it. So I followed the instructions, plugged into my PC, opened the BBB as an external drive and opened t...
    Profile Photo
    last modified by Duncan Fraser
  • BBONE-BLACK-WIRELESS and BB-CAPE-DISP-CT43

    Hello, I am trying to figure out if the two products in the subject line are compatible without having to jump through those proverbial hoops: the element14 BeagleBone Black Wireless with WiFi & Bluetooth, and th...
    Profile Photo
    last modified by teddytronix
  • Do I have a bad BB-AI? Suggestions Welcome

    I've had my BB-AI a couple weeks, and I'm running from the on board eMMC with debian 9.9 just fine, The tidl examples work.  But I wanted to flash the newer 'buster' image.  It does not work.  I read al...
    Profile Photo
    last modified by mp2100
  • Odd PRU interrupt behavior

    I want to determine if I can use the PRUs to interact with an instrument for a satellite payload. I am able to get rpmsg-proc working and can move blocks of data quickly enough. I added the IEP timer and want to set i...
    Profile Photo
    last modified by ivangalysh
  • Use UART0 of pocketbeagle, disable boot and console

    Hi, I have designed a PCB with pocketbeagle as a module, I made a mistake and instead of UART 4 I have connected UART 0, before I cut tracks, I would like to explore option of using UART 0 for my application and UART4...
    Profile Photo
    last modified by chrischristian14
  • BeagleBone® White HDMI Cape by Embest

    This product is likely end of life. This document is here purely for support purposes should the files be required if anyone has the add-on cape.   The BeagleBone-HDMI Cape is designed by Embest to provide HDMI ...
    Profile Photo
    last modified by Christopher Stanton
  • Coding for the BeagleBone PRU with C in 2019

    So, I've recently decided to get my head around the killer feature of the BeagleBone family - the two Programmable Realtime Units that sit alongside the ARM Cortex A8 core that you'll normally find running Linux. Thes...
    Profile Photo
    last modified by Fred27
  • USB 3.0 support for beagle bone AI.

    I want to use basler ace camera (acA1300-200um) with beagle bone AI board. It requires usb 3.0 host controller. As BB AI board provides only usb 2.0 , camera isn't working. Is there any way we can add usb 3.0 support ...
    Profile Photo
    last modified by prathamesh12
  • Reading BeagleBone AI Temperatures

    I finally brought up my BeagleBone AI with a 25mm x 7mm fan firmly screwed into the heat sink using M2 or M3 (they were salvaged so I don't know for sure) machine screws. It was a lot quieter than I was expecting al...
    Profile Photo
    last modified by gdstew