Skip navigation
Charlotte Godley presents the next episode of 'Circuits with Charlotte' in which she demonstrates some of the features of the RIoTboard by Freescale.   See the product here: http://bit.ly/1Ci1A3A   ...
In a previous blog series we have build u-boot, kernel and packages for  Riotboard using Yocto.   This time we shall use the Yocto Gui based BSP and QT to create a simple camera application.   Hardware Requirements: 1. RIoTboard 2. LCD8000-97C (LVDS) or HDMI 3. CAM8000-D   I am using LVDS display for this guide, you can use HDMI. make sure to change boot params accordingly.   Download the BSP from here , unzip it and flash to sdcard.   Now connect the cam80 ...