Skip navigation
This post documents a recent build of Android 4.3 Jelly Bean for RIoTboard on a fresh installation of openSUSE 13.2 x86_64. The build images were transferred to an SD card using Linux commands rather than using the MFGTool.   HARDWARE AND BUILD OS   Gateway NE56R12u Laptop running openSUSE 13.2 x86_64 DVD      2.1 GHz Intel B950 dual-core Pentium processor      8 GB physical RAM      135 GB /home partition for build  ...
This post documents a recent build of Android 4.4.2 KitKat on a fresh installation of openSUSE 13.2 x86_64 using the Element14-provided source code for RIoTboard. The build images were transferred to an SD card using Linux commands rather than using the MFGTool.     HARDWARE AND BUILD OS   Gateway NE56R12u Laptop running openSUSE 13.2 x86_64 DVD      2.1 GHz Intel B950 dual-core Pentium processor      8 GB physical RAM     ...
This post documents a recent build of Android 4.4.2 KitKat on Ubuntu 12.04.5 LTS x86_64 Desktop using the Element14-provided source code for RIoTboard. The build images were transferred to an SD card using Linux commands rather than using the MFGTool.  Ubuntu 14.04.5 LTS x86_64 Desktop users should see the Addendum at the bottom of the post for additional information.   HARDWARE AND BUILD OS   Gateway NE56R12u Laptop running Ubuntu 12.04.5 LTS x86_64 Desktop    & ...