• Getting Started:  RIoT Board

    Watch as an element14 Product Specialist gets started using RIoT Board.
    Profile Photo
    created by pchan
  • RIoTboard always starts in recovery mode!

    I started working on RIoTBoard recently for learning purpose. My develop environment is Ubuntu 18 and I'm trying to follow the steps mentioned in this link. When I try to boot the board with SD card or uSD card, with...
  • Linux 4.1 + Ubuntu 14.04 on RIoTboard

    Intro I was inspired by Otto's blog series of getting Debian Linux on the RIoTboard: Linux on the RIoTBoard Part 1: U-Boot. However I need Ubuntu instead.   Following are the steps to get a current Linux kernel ...
    Profile Photo
    last modified by create
  • RIoTboard BSP Images and Tools Download - Android and Linux

    Android Linux BSP JellyBean v4.3 SDcard Image Download Image Download BSP Linux Ubuntu v3.0.35 SDcard Image Download Image Download BSP KitKat v4.4 SDcard Image Download Image Download BSP Linux Yocto v3.10.1...
    Profile Photo
    last modified by Christopher Stanton
  • Riotboard doesn't recognize Wi-Pi

    Hi, I have a Riotboard with Ubuntu booted from an SD card, I been trying to use a wifi connection with the Wi-Pi module but it doesn't work.     When I plug it in and run the lsusb command on terminal it sh...
    Profile Photo
    last modified by jorgerito
  • Ubuntu 14.04

    How can I install an the actual Ubuntu 14.04 or at least how can i fix the reboot problem at ubuntu 12.04. Has anybody a finished image available for download, in order to use with the riotboard.?
    Profile Photo
    last modified by e_b_123
  • RIoTboard: Building a TFT LCD Display and Digitizer - Part 2: Circuit

    Part 2: Introduction This project is about connecting a screen from a laptop to the RIoTboard. For a full introduction, see part 1 by clicking here, it goes into more detail about this project. This part 2 covers the ...
    Profile Photo
    created by shabaz
  • internet connection

    HI the riot board is not connecting to internet .I used both wi-fi dongle and ethernet connection and also i configured edit connection.
    Profile Photo
    created by nandhish
  • to use uart4 and uart5

    I am a new user to riotboard and ubuntu so i cannot find this (/linux-imx/arch/arm/mach-mx6/board-mx6dl_riot.h) in any of the root files and also am not able to flash through emmc so i am  using sd card.plese som...
    Profile Photo
    created by nandhish
  • to use uart4 and uart5 in ubuntu linux

    I don't know how to use uart4 and uart5 .the ttymxc3 and ttymxc4 is not showing in the device and also my riot board is not connecting to ethernet so i need to know how to use the uart4 and uart5 since i have used...
    Profile Photo
    created by nandhish
  • Metal Enclosure for LCD8000-70T

    This post describes a project to place an Embest LCD8000-70T 7-inch display in an aluminum enclosure suitable for use with a similarly enclosed RIoTboard SBC.   References   Metal Enclosure for RIoTboard ...
    Profile Photo
    last modified by stmorgan
  • Metal Enclosure for RIoTboard

    This post describes a metal enclosure suitable for use with the RIoTboard provided you have some time and access to the proper tools.   I have been looking for an enclosure for my RIoTboard for a number of reaso...
    Profile Photo
    last modified by stmorgan
  • Serial console output is not coming

    Hi, I have flashed linux kernel 3.10 available on the riotboard . Through ssh I am able to log in to the device. But I am unable to get the serial console output . I am using usb to serial cable (6 pin out). I b...
    Profile Photo
    last modified by harshrao464
  • Rooting Android for the RIoTBoard

    I´m not an Android developer. I´m using my RIoTBoard mainly with a Debian Linux distribution. but because I am rooting all of my Android devices, I thought why not root the RIoTBoard as well. Just for fun...
    Profile Photo
    last modified by radiatortwo
  • Riotboard: IoT based intrusion detection & alert system: Part2 : Capturing image

    In this mini blog series we will build an IoT based intruder detection and alert system.   Blogs: Part1 : Connecting Pir Sensor Part2 : Capturing intruder image  <--- this blog Part3 : Email Alerts &...
    Profile Photo
    last modified by tushar panda
  • Kali on RIoTBoard....its possible?

    Did someone managed to install Kali <<https://images.offensive-security.com/arm-images/kali-2017.3-riot.img.xz>> on RIoTBoard? I followed the instructions from <<https://docs.kali.org/kali-on-arm/ka...
    Profile Photo
    created by epsylon67
  • Old Android Tablet as a Riotboard display

    I have a Polaroid tablet running android 4.2.2   Is there a way to use the tablet as a display for the RIoTboard?  I'm in a college class and I live about 40 miles away.  My lab partner and I both live...
    Profile Photo
    created by mrpipes3
  • Problem on RioT Board Compilation

    Hi,    In our Corporate network Git is blocked, So while compiling I had below error, ERROR: Function failed: Fetcher failure for URL: 'git://github.com/philb/update-rc.d.git'. Unable to fetch URL from any...
    Profile Photo
    last modified by santhoshkarthiktce
  • Compilation Procedure to get *.sdcard file in RIOT board

    Dear Mentor,   While I am compiling the Linux Source using Yocto, I am not getting *.sdcard file. but I am getting Uboot, Uimage and RFS. Can you please let me know if any commands needs to be added while compil...
    Profile Photo
    last modified by santhoshkarthik
  • debug/repair riotboard powerup

    Hello,   I haven't been using the riotboard for a while, and now it does not power up anymore (the green LEDs are on, but there is no boot signal on the screen).   Is it possible to repair the board, e.g. ...
    Profile Photo
    last modified by farsi