Skip navigation

MiniZed

2 posts
In Path to Programmable Blog 7 - Trying out a PL-only VGA design & Path to Programmable Blog 10 - MiniZed does DVI/HDMI, I used the MiniZed that was sent to the Path to Programmable challengers to generate VGA & DVI/HDMI video.   Continuing with video related FPGA projects, I decided to attempt two more: Use the FPGA to drive a LCD panel that I salvaged from an old laptop Implement a HDMI sink on the FPGA, and send the incoming video the LCD panel.   This blog post covers t ...
1. Introduction I have a really nice sensor module called GDK101 which allow to measure a gamma radiation in range up to 200 usV/h. This sensor have really simple communication interfaces: I2C or UART. There is also analog output which could be used for verifying the energy spectrum analysis of gamma photons. Below there is typical connection circuit: Sensor module has sensitive 10 PIN photodiodes and transimpedance amplifier circuit. In functional block diagram there is also comparator and p ...