• Microzed USB configuration for petalinux 2018

    Hi all,   I can see many discussions in the forums about getting USB host-mode working on a Microzed (Zynq 7020). In particular, here's a selection of links that I've already read:   http://zedboard.org/co...
    Profile Photo
    last modified by maldata
  • Network FMC card - Industrial Ethernet

    Hi, I am a novice and have currently started working with the microzed industrial ethernet kit.  I was able to run the ethercat demo version on the board using the network fmc module, however, I ...
    Profile Photo
    last modified by bbhatt
  • MicroZed Industrial IoT Starter Kit

    The Avnet MicroZed IIoT Starter Kit enables hardware and software developers to create and evaluate Zynq™-7000 All Programmable SoC designs, using on-board sensors to gather information from the immediate surrou...
    Profile Photo
    last modified by troutchaser
  • Missing tutorials from MicroZed IIoT

    Hello, I would like to know if there´s a special reason on the removal of the tutorials that were available at:  http://zedboard.org/support/design/13591/116   I was/am following some steps and usi...
    Profile Photo
    last modified by joaomota1994
  • Microzed Hello world

    Hi, I try to run the 'Hello World' project on Microzed. After successful FPGA programming, in the 'lunch on hardware part', I got this error:  DAP status f0000021 AP transaction error, DAP status f0000021. ...
    Profile Photo
    last modified by m.khalafian@primes.de
  • Accessing Arduino expansion card I/O

    I wish to connect ST X-Nucleo audio card X-Nucleo-CCAO21 to Arduino Carrier Card and access its signals (I2S) using the MicroZed module.  Is there a tutorial that can help me get started on this?
    Profile Photo
    last modified by rahuldee
  • MicroZed IIoT Blog Post

    Here's some reasons why you might want to consider this kit for your next IoT project: http://ibm-iot-blog.com/microzed-industrial-iot-starter-kit/ Ron
    Profile Photo
    last modified by hockeyman1972
  • Restart everything

    Hello! i've tried to boot the wind river linux from sd card . i've everything like new except for the booting instructions! First question: do i need to download an iso image and burn it to SD Card in order to sta...
    Profile Photo
    last modified by joaomota1994
  • Communication of I2C devices with Zedboard

    As I am a beginner in Zedboard - Zynq®-7000 I need to know How should I install the I2C library in zedboard to create the communication between I2C sensors and Zedboard Is there any tutorial whi...
    Profile Photo
    last modified by bart23
  • Generate new boot.bin

    Hi, I have a picozed board that I am working with, and I have gone through the tutorials with the microzed IIoT kit to see how to interface Wind River Pulsar with my designed PL. When going through the tutorial for t...
    Profile Photo
    last modified by rscordeau
  • Can't find the files for the quick start example

    Hello ! I had to reformat the SD card. I am trying to finish the quickstart but i don't find the files to execute. Whenever i plug the SD card to my pc i get 3 different partitions.  I found the Quickstart...
    Profile Photo
    last modified by joaomota1994
  • Access the USB in Microzed Board

    Hello, I'm using Microzed evaluation kit for my development of interface card. Burnt Pulsar Linux OS given as per instruction.  Problem: I'm not able to get the device address of USB (which is just below t...
  • SD Card

    I messed up the micro SD boot information, can someone give me the original image that came with it?
    Profile Photo
    last modified by joaomota1994
  • Missing drivers

    Hello! I'm guessing that i have problems with missing drivers this time.  The last time I was having problems with the fact that i had to reset the board and lost all of the code files of the example code. I go...
    Profile Photo
    last modified by joaomota1994
  • Microzed-Petalinux

    Hi,   I am a novice in the field of networks and wanted to know if there are any packages available on petalinux that would allow me to work on the individual ethernet packets (manipulation of the packets)...
    Profile Photo
    last modified by bbhatt
  • microzed to memory interface

    I want to read memory data with specified frequency continuously and write to a IO's(12bit data).     MY DOUBTS ARE : How to fill 64k samples of data into memory , where to fill this data so that am ...
    Profile Photo
    created by ssudi