• hello world not working minized

    Hi.   I am trying to run the helloworld example on the Minized. I have followed multiple tutorials but no one works. I manage to run the petalinux and I see it in Putty. This means my UART cable is working and ...
    Profile Photo
    last modified by relise
  • minized lab files?

    I started on the MiniZed Lab/Training today, but it looks like the hardware files (Vivado Project files) aren't in the ZynqDesign subfolder. Is this an oversight? Were the files intentionally removed from the download...
    Profile Photo
    created by pshepherd
  • the link zedboard-ov7670 has been deleted of hamsterworks. how can I have this file?

    Hi dear The link of zedboard-ov7670 file has been deleted of hamsterworks. how can I have this file? Thank you
    Profile Photo
    last modified by quantom3230
  • length for each IO on FMC for UltraZed-EV Carrier Card

    Designing an FMC Daughter Card to work with the UltraZed-EV Starter Kit. I found the length data in UltraZed-EV SOM, but I did not find it in UltraZed-EV Carrier Card. Can you specify length the length for each IO o...
    Profile Photo
    created by xchjg
  • 2019.2 petalinux BSP for MicroZed

    Is there a plan to release a MicroZed 7020 BSP for PetaLinux 2019.2?
    Profile Photo
    last modified by astromorgan
  • How to install Android on Zedbord?

    I search google find this topic, but this document is too old. could guys install Android on Zedboard? https://elinux.org/Zedboard_Android
    Profile Photo
    last modified by dolanna
  • Pre Requisites to Start Working on MicroZed Board

    Hi Members,                I would like to know the Pre requisites to start working on MicroZed Board. 1) Micro Zed Board 2) Micro USB Cable, 3)...
    Profile Photo
    last modified by ganesh_b
  • XADC temperature reading issue

    I am trying to use XADC on Zynq. Using Vivado hardware manager I look at XADC and see Temp is -273. I checked VCCADC, it is 1.8V as shown in the schematic. I check Arty board, and I can get 25 degrees C. I am afraid a...
    Profile Photo
    created by frankqwu
  • Do you have back-up files from the SD-card ZedBoard to download them?

    I try to start the ZedBoard setup and basic operation, but it never loads the files. I think the memory card is damaged or the files don't work properly. I want to repeat the process with a new memory card and files r...
    Profile Photo
    last modified by eduardoibarra-medel
  • Given that this particular site is labeled as ZedBoard training where is the training?  The name and function should match.  This looks like a discussion forum.

    Thank You Nick
    Profile Photo
    last modified by nick0559
  • MiniZed seems very dead

    I am totally new to zedboards and fpga systems and SoCs like this in general, so sorry if this seems silly:   I was trying to run a hello world project on my MiniZed board when I accidentally diconnected the usb...
    Profile Photo
    last modified by sigurdht
  • Trying to build a Vivado bitstream for the minized+Petalinux

    Hi all, I am trying to find a .bsp file that will create a bitstream to use with PetaLinux. I tried minzed_ttc_2019_1.bsp When I open the project I get a number of missing vhdl modules which I found on the Avnet gi...
    Profile Photo
    last modified by 100charlesb
  • where can I find speedway training lab files?

    My customer is specifically looking for LAB 9 of the Avnet Zynq Software Speed way design course” details how to make a dual core application in which both run bare metal.
    Profile Photo
    last modified by seema.simon@avnet.com
  • MiniZed JTAG FTDI FT2232 Programming (FT_PROG)

    The JTAG circuitry used on the Avnet MiniZed is a Xilinx solution based on the FTDI FT2232. As stated in https://www.xilinx.com/support/answers/68889.html, "the proprietary solution is not documented or supported, and...
    Profile Photo
    created by bhfletcher
  • MicroZed microSD card image archive failing virus scan

    I tried to down load the archive from this page, but it seems to be failing the on-site virus scan. I've tried a few times with the same result. MicroZed Linux microSD Card Image Archive   Error message: There...
    Profile Photo
    last modified by Fred27
  • Petalinux failes when configuring U-boot environment

    So when I attempt petalinux-build after configuring u-boot with Environment -> Environment in an MMC Device enabled. It fails to build.     make[1]: Leaving directory '/home/mascenzi/Development/petalin...
    Profile Photo
    created by nightpoison
  • Workshop "Integrating Sensors on MiniZed with PetaLinux 2019.1" - missing files

    I just started this free online course and tried to follow this instruction in LAB1 "2. From the host OS (Windows), locate the minized-petalinux-AvnetTTC-labs.tar.gz lab files archive within the Support_documents fold...
    Profile Photo
    last modified by olebon
  • Can a Zedboard be used without adding a Zynq processor?

    I have used the Zedboard as a processor with custom hardware, no problem.  Is it possible to start from the other end?  For instance, the most trivial case would be hooking up a Constant IP with 8 bits to th...
    Profile Photo
    last modified by radlyeel
  • Petalinux - MiniZed packages not visible rootfs

    Hello!   I have small problem with visibility of meta-user packages.   I have copied all "project-spec/meta-user/*" files from BSP 2019.1 to 2019.2 and I can't see any new fields in "petalinux-config -c ro...
    Profile Photo
    last modified by bartokon
  • Trusty MiniZed Finally Bit The Dust

    Hello I'm getting no activity through TeraTerm My power LED is on, My two, once blinky, LEDs are both glowing a depressing shade of ORANGE. My power connections are correct. Apart from finding a version of Vitas ...
    Profile Photo
    last modified by johnkeeling