• Ultra96 Anyone tried to use the HS Connector with 1.8V logic

    I am aware that the HS connector uses 1.2V logic but is there a way to bodge it to operate with 1.8V logic? I notice the VCCO_HP rail is powered by a TPS6508641 (LDO03A) which can be programmed to 1.5 volt then look...
    Profile Photo
    last modified by 100charlesb
  • Error booting from SD card

    Hello,   I'm using an UltraZed IO Carrier Card. I have used my custom Petalinux with no problems. But since yesterday, I don't know why, it doesn't boot from the SD Card. Also I have tried with the UltraZed IO C...
    Profile Photo
    last modified by qarlosalberto
  • DDR4 speed typo in UltraZed-EV HWUG?

    Hi,   In the hardware user guide here:    http://zedboard.org/sites/default/files/documentations/UG-AES-ZU7EV-SOM-G-V1.pdf I read that DDR4 RAM can do 2400 Mbps (mega bits/sec) transfer speed. Is th...
    Profile Photo
    last modified by buckd
  • petalinux 2019.1 build error with ultrazed EV 2019.1 bsp

    Hi   I am using the Xilinx petalinux tool version 2019.1 to build the images for booting up the Ultrazed EV starter Kit. I have downloadedUltraZed-EV Carrier Card—PetaLinux 2019.1 Enhanced BSP file from t...
    Profile Photo
    last modified by jkmenon-ign
  • UltraZED-EV + IO Carrier Card VCU in 4KP60

    Hi,        I read the post (UltraZED-EV + IO Carrier Card VCU Design Example (v2018.3)) by Jason Moss about his test on the ZynqUS+ VCU. It seems the highest resolution he tested was 1080P30....
    Profile Photo
    last modified by simontam1234
  • UltraZed USB 3 IDS Camera Speed Issue

    We have the UltraZed eval board (EG) and have Xilinx 2017.4 u-boot/kernel with Ubuntu 18.04 running.  USB 3 seems to be setup correctly - all USB 3 devices we've tried are recognized as USB 3.  We are connec...
    Profile Photo
    last modified by jbspears
  • UltraZed-EG bsp 2019.2 not working

    Hello,   I downloaded UltraZed-EG IO Carrier Card - PetaLinux 2019.2 Enhanced BSP  file for petalinux 2019.2 but it is not working, I can't create a project with this file. I got following error when creat...
    Profile Photo
    last modified by jonathanc
  • lwip autonegotiation fails when using FSBL

    Hi, I have a Vivado design based on UltraZed-EV SOM. I am using Vitis 2019.2 to develop an application that makes use of a lwip TCP server. It happens that if I launch the application by selecting the psu_init.tcl fil...
    Profile Photo
    last modified by dat63
  • UZEV USB as host and custom carrier card, problem with USB_OTG_CPEN held low

    Hi,   We are designing a custom carrier card for the UZEV and we have a problem with the USB interface with the USB_OTG_CPEN pin always held low. We want to use it as a host and we have the following setup: ...
    Profile Photo
    last modified by buckd
  • UltraZed EV No longer detects JTAG devices

    I've been using an UltraZed EV board for software development, using the Xilinx toolchain for months, without many problems. This week, I can no longer detect any devices under the JTAG chain. I've tried several diff...
    Profile Photo
    last modified by wdf
  • Avnet Vitis platform build for UZ7EV_EVCC error

    Hello,   Running the make build script from the Avnet/Vitis repository is causing some problems. My machine is a Ubuntu 18.04.1 LTS VM. I have the latest and greatest toolchain versions 2019.2 (Vitis,Vivado and...
    Profile Photo
    last modified by kvanwezemael
  • Ultrazed-EV SOM + Carrier card + Xilinx Echo server on SFP issue

    Hi, I am trying to enable the SFP+ interface 1 by connecting it by RJ45 to SFP+ converter and run the XIlinx echo server on it. In my Vivado design, I used the AXI 1G/2.5G Ethernet subsystem with the GT reference c...
    Profile Photo
    last modified by clc1717el14
  • UltraZed-EV starter kit kernel boot problem.

    Hello!   I have the UltraZed-EV System-on-Module Starter Kit. I have the petalinux-2019.1 and UltraZed-EV Carrier Card—PetaLinux 2019.1 Enhanced BSP.   I created a project and checked that the root ...
    Profile Photo
    last modified by dpechkin
  • USB 3 devices only detected with USB 2 speed

    I’m trying to get a USB 3 device working on the UltraZed I/O Carrier Card with an UltraZed-3EG SoM. The device is usually detected, but only as a USB 2 full-speed device. The USB drive I’m using for testin...
    Profile Photo
    last modified by svonohr
  • Display Port issue on Ultrazed 7EV SOM+Carrier Card

    We bought two Ultrazed 7EV SOM+Carrier Card starter kits. I cannot get the display port to work with the shipped SDCARD as is, and looking for some help.   I followed the avnet 7ev cc test document and display p...
    Profile Photo
    last modified by ontran
  • HDMI In and Displayport out

    Hello,   I wonder if someone has done a pipeline from HDMI in and Displayport out on the Ultrazed? No VCU, yet.   The Avnet 2018.3 Example Design used ZCU106 TRD but stripped out hdmi as an example. What's...
    Profile Photo
    last modified by ontran
  • Ultrazed EG starter kit boot problems + jtag problems

    Hi. I have an Ultrazed EG starter kit which fails on boot with this serial output: Avnet modifying SDHCI0 and SDHCI1 registers for UltraZed SOM   SERDES initialization timed out XFSBL_PSU_INIT_FAILED =======...
    Profile Photo
    last modified by benka
  • IDT Versaclock programmation

    Hello, I'm designing my own custom carrier board to support the UltraZed SOM and I planned to use the same IDT clock generator used on your IOCC carrier board. The reference indicated in the BOM is 5P49V5935B521LTGI...
    Profile Photo
    last modified by sonictai
  • Pynq support for Ultrazed EV

    Hello,   I was wondering if any offical board support for the PYNQ envirnonment -like for the ZCU104- is planned or underway.   With kind regards,   Kris
    Profile Photo
    last modified by kvanwezemael
  • UltraZed-EV and Petalinux-2019.2

    Hi experts,   I'd like to know where I can find the BSP for UltraZed-EV for using with Petalinux-2019.2, please?   Thanks in advance, Khang
    Profile Photo
    last modified by khangdnl