• fpga programming using Ubuntu 18.04

    Hello,   I am testing a mini-itx board with Ubuntu 18.04 host OS.   The tests with builtin software went ok. However, when i try to program the FPGA via this module https://store.digilentinc.com/jtag-smt2...
    Profile Photo
    last modified by amamory
  • iam using mini-itx-7z-asy-g avnet zynq-7000 soc processer in that i want know about uart implementation in this board i found only one usb-uart bridge i want implement the uart protocal on this board using xilinx vivado and xilinx sdk plese help out me fr

    iam using mini-itx-7z-asy-g avnet zynq-7000 soc processer in that i want know about uart implementation in this board i found only one usb-uart bridge i want implement the uart protocal on this board using xilinx viva...
    Profile Photo
    last modified by naresh99
  • Issue with PSiP Power Module of Mini-ITX-7Z-ASY-G

    Hi all, We have a Mini-ITX-7Z-ASY-G board, it is connected to the power module Panasonic PSiP. I have an issue that when I turn on the FPGA board, the power module doesn't turned on and it doesn't work. Can you pleas...
    Profile Photo
    last modified by nafiseh
  • Zynq 7100 PS lockup

    It appears that when I get to a certain utilization of the Z7100 device in the PL it will cause the PS to lockup where I cannot get access to the PS through the serial port.  I do see that the logic in the PL is ...
    Profile Photo
    last modified by 100billgood
  • Power Rails monitoring

    Hi,   Is there a way to monitor power rails for PS and PL on Mini-ITX board. I have monitored power on ZC702 using a TI adapter connected to the board before. I wish to do something similar on Mini-ITX. Is ther...
    Profile Photo
    last modified by umar_minhas
  • mini-itx DDR problem

    I recently purchased a mini-itx100 system and am having trouble getting it to boot. None of the pre-packaged designs seemed to word(sd card or qspi flash), but the JTAG connection works ok, so I tried building some of...
    Profile Photo
    last modified by jenn.holt
  • 7-inch Display Kit in Linux

    Hi, I'm working with a Zynq Mini-ITX dev board and the following display kit:   http://zedboard.org/product/7-inch-zed-touch-display-kit   The display kit provides a boot image with a bare-metal applicat...
    Profile Photo
    last modified by mkipper
  • Initial Startup

    Hello all, I purchased a MIni-ITX recently, and I guess it was just the FPGA board alone not realzing I needed a power supply and everything else. So I rigged up an ATX Power Cable that has 12V, 5V, and 3.3V coming o...
    Profile Photo
    last modified by electrodev99
  • Mini-ITX self-test - PL DDR issue?

    Hello everyone, Just wondering whether there's a self-test boot image available for the 7045 mini-ITX board. I'm seeing some odd behaviour (more below) which I'm 99% sure it just a configuration/software error but I'...
    Profile Photo
    last modified by evan-slatyer
  • ZYNQ PCIe Root Complex issue

    My customer design a Root Complex mode based ZC7015 refering AVNET Mini-ITX RC PCIe reference design. But we meet initial failed issue. The attachment is UART info. Can you give some advice about it? U-Boot 2013.04 (N...
    Profile Photo
    last modified by goldsunmonkey
  • Linux build for mini itx

    Hello Where can I download linux software for building mini itx image? Is it with petalinux? Is there any wiki or document how to create image for the board ? Regards Ran
    Profile Photo
    last modified by 100ranran
  • Building U-Boot

    The instructions and source files in both: Zynq_Mini-ITX_z7100_Ubuntu_FAT_v2014_4_0.zip and Zynq_Mini-ITX_z7100_Ubuntu_FAT_v2013_4.zip Are incorrect and I can't build U-Boot for this board (Zynq Mini-ITX z7100). ...
    Profile Photo
    last modified by andydracup
  • 3.17 Kernel hang

    Hello, We are currently running M-ITX platform with modified PCIe root complex design and patched up Linux kernel (2014.4) 3.17 version. We have a Nvidia GPU sitting in the PCIe slot and lspci shows the device with...
    Profile Photo
    last modified by h@qdi
  • Mini ITX not showing USB ports

    Hi All, For a project I am trying to get the Zynq_mini_itx up and running with USB ports. Used the zynq_mini_itx_board_filesv2015_3.zip and followed the manual. I managed to get a working image however the USB port...
    Profile Photo
    last modified by 100maverick2k
  • usage of qspi pins by programmable logic

    Can QSPI pins be used by the programmable logic? ug585-Zynq-7000-TRM.pdf, figures 2-3 and 2.-5 show programmable logic connected through EMIO block to MIO mux which implies that EMIO signals could connect to the same ...
    Profile Photo
    last modified by arturd1
  • PS not responding

    Hi, I am trying to run a simple helloworld+led-blink application on the Mini-ITX. I have tried JTAG, QSPI, and SD Card configuration, with varying results. Using JTAG, I am able to program the PL, but the PS does n...
    Profile Photo
    last modified by ctfelten
  • Mini-ITX Turns off after Power On

    I have purchased the Mini-ITX development board but the unit turns off within seconds after power on. There are no issues with the ATX power supply. I would like suggestions on how to troubleshoot the issue.
    Profile Photo
    last modified by rsahakian
  • booting miniITX usb uart interface

    Hi , I would like to know if it is possible to load the linux OS to miniITX board through the USB_UART interface when it is powered ON?. Do let me know the procedure if anything exists. The only way to load linux to...
    Profile Photo
    last modified by miniitx_learn
  • PCIe problems when using USB 3.0 cards

    Hi, I'm trying to get USB 3.0 running through the PCIe slot. I have been using two different USB 3.0 cards, one with a NEC and one with a VLI chip, but have experienced (different) problems with each. My hardware des...
    Profile Photo
    last modified by cone83
  • Ethernet only working in Gigabit mode (not 100Mbit/s)

    I have a Gigabit ethernet card in my primary development computer. When I connect the Mini-ITX Zynq board directly to that (with static IPs on both), it works fine (testing with "ping <address>". However, if it ...
    Profile Photo
    last modified by sam.jaeschke