Skip navigation

Autodesk EAGLE

2 Posts authored by: yahyatawil
Hello   I used negasilk.ulp for a while for inverted silkscreen, but I decided to enhance it a little and make it easier.   Steps:   1. First create your art work (Polygon in top layer with text inside it on layer 41 tRestrict with vector font type). 2. Run Ratsnest. 3. Name the polygon with "NEG_SILK" to make it special from other normal polygons.   With this enhancement there are no need to run any script file and also can help you to add negative silk screen with ...
LibIt ULP This ULP makes creating packages for libraries much easier. You can use is to draw multiple SMDs/PADs, lines and rectangles PAD Dialog has the following options: Select Shape: Select the shape of pad (Square-Round-Octagon-Long-Offset). Select Axis: Select the axis of pads. Adding them horizontally or vertically. Select PAD Angle: Select the angle of pad (0-45-90-180). Count of PADs: Select how many pads you want to add. Pitch (Distance): Select the distance between every 2 pads. ...