Skip navigation
Webinar Video Q: Is this project summarized in a single Elektor magazine? A: Yes, in the December 2014 edition. Q: Can I buy the kits/built boards via Element 14? A: No, they are sold by Elektor (www.elektor.com) Q: Which controller is being used, please? A: LPC812M101JDH20FP (TSSOP20) Q: is the rotary encoder optical? A: No, it has sliding contacts. Q: 16K bits or bytes of flash? A: 16 KB i.e. bytes Q: Hi Clemens! Does the mcu can provides PWM outputs to drive a full bridge for motor control? ...

Filter Blog

By date: By tag: