Ben Hecks Lunchbox Dev Kit Remixed
by MAYER MAKES

[Scrolle runter um die deutsche Version zu lesen / Scroll down to read the german version]
 

Have you ever wanted to recreate one of Ben Heck‘s projects in your own style?

I certainly did, and when I was given the opportunity to remix a project from the Ben Heck show, I had no time to waste.


 

I‘m Clemens Mayer , austrian maker and host of the youtube-channel MAYER MAKES (german language), which features content including electronics projects, 3D printing, reviews and maker community events and all kinds of DIY topics.

The video is in german but you can turn on english subtitles.


 

[VIDEO]


 

Recently I had the chance to remix one of Ben Heck‘s latest projects, the Lunchbox Dev kit.
I gave it the austrian treatment by massively overpowering it, while completing the project on the lowest budget possible.

The MAYER MAKES version of the Lunchbox Dev Kit supports up to 10 developement-kits or single board computers at once, while providing various networking options.
It features a built in VGA screen with CFFL-Backlighting, which is converted to accept HDMI signals from the connected devices. It took 3 VGA monitors, to create one working unit, due to weird power supply failures and strange glitches.
Did I mention it consumes up to 450W ? No chance to run it on batteries as long as you want to be able to lug it around.
Element 14 provided the most vital parts, for example the power supply, HDMI converter, Beaglebone Black boards and 3d printing filament.
When the space inside the case got really tight, they saved the project with a very compact keyboard/mouse combo.

If i would ever rebuild this unit I would take the extra time and replace the CFFL tubes with LED backlighting to cut down on power consumption. Maybe 5 dev-kits at once would be enough for IOT-developement,and some additional storage for components could be useful.
I guess the Lunchbox dev kit may help with covering the world in IOT-devices whatever they may be good for. ;-)

I would love to remix some more of Ben Heck‘s projects, like portable game consoles.Taking my spin on the junk keyboard, by digitizing a guitar or remixing the Nintendo-playstation prototype by actually building a game console that never was, but could have been.
With the Help of Element14 those ideas could turn into reality and great episodes.

 

What is your opinion on my remix of the Lunchbox dev kit?
Are there any projects you want to see remixed by MAYER MAKES?
Let me know on the Element14 community or social media:

 

Element14: @MAYERMAKES

youtube.com/mayermakes

facebook.com/mayermakes

twitter.com/mayermakes

instagram.com/mayermakes

 

GERMAN Version Deutsche Version

 

Ben Hecks Lunchbox Dev Kit Remixed
von MAYER MAKES


 

Wolltest du jemals eines von Ben Heck‘s Projekten in deinem eigenen Stil nachbauen?

Ich wollte das unbedingt und als Element14 mir die Möglichkeit dazu gab, hatte ich keine Zeit zu verlieren.


 


 

Ich bin Clemens Mayer, Maker aus Österreich und Hauptakteur auf meinem Youtube-Kanal MAYER MAKES (deutschsprachig), auf dem ihr verschiedene Videos zu Elektronik-Projekten, 3D-Druck, Reviews und Maker-Community-Events und vieles mehr rund um das DIY-Thema findet.


 

Das Video ist auf deutsch und es gibt englische Untertitel.


 

[VIDEO]


 

Vor kurzem hatte ich die Chance eines von Ben Heck‘s Projekten nachzubauen und zwar das Lunchbox Dev Kit.
Ich habe ihm die österreichische Behandlung gegönnt, nämlich gewaltig übertriebene Leistung bei möglichst kleinem Budget.

Die MAYER MAKES Version des Lunchbox Dev Kit unterstützt bis zu 10 Developement-Kits oder Einplatinenrechner auf einmal und verbindet sie mit verschiedenen Netzwerkmöglichkeiten.
Enthalten ist ein VGA Bildschirm mit CFFL-Hintergrundbeleuchtung, der modifiziert wurde um HDMI-Signale der angeschloßenen Geräte verarbeiten zu können. Ich habe auf dem Weg ein funktionierendes Gerät herzustellen dank merkwürdiger Netzteilfehler und seltsamer Schwierigkeiten beim Umbau 3 VGA-Bildschirme zerstört.
Habe ich schon erwähnt, dass das Lunchbox-DEV-KIT 450W verbraucht? Keine Chance, dass dieses Ding jemals auf Batterien läuft, ausser man verzichtet auf die Möglichkeit es noch transportieren zu können.
Element 14 hat die wichtigesten Teile zum Beispiel das Netzteil, HDMI-Converter, Beaglebone Black Boards und 3D-Druck-Filament für dieses Projekt zur Verfügung gestellt,
Als der Platz im Koffer wirklich eng zu werden drohte, haben sie das Projekt mit einer kompakten Tastatur/Maus-Kombination gerettet.

Wenn ich dieses Projekt noch einmal bauen könnte, würde ich mir die extra Zeit nehmen und die CFFL-Hintergrundbeleuchtung durch LED-Leisten ersetzen, um die Leistungsaufnahme zu verringern. Vielleicht wären auch 5 Dev-Boards genug und etwas Platz für Bauteile könnte auch nicht schaden.
Ich glaube das Lunchbox Dev Kit könnte durchaus dabei helfen die Welt mit IOT-Geräten einzudecken, was auch immer die dann genau für einen Zweck haben. ;-)


 

Ich möchte sehr gerne noch mehr von Ben Heck‘s Projekten remixen: zum Beispiel eine tragbare Konsolen. Ich würde meine Runde am Junk Keyboard durch eine digitalisierte Gitarre aufmotzen oder den Nintendo-Playstation Prototyp aufleben lassen in dem ich eine Konsole baue, die es nie gab, aber geben hätte können.
Mit der Unterstützung von Element14 könnten aus diesen Ideen bald echte Projekte und großartige Episoden werden.

 

Wie findet ihr mein Lunchbox Dev Kit?
Welche Projekte würdet ihr gern von MAYER MAKES remixed sehen?
Schreibt mir in der Element14-Community oder in den sozialen Medien:

 

Element14: @MAYERMAKES

youtube.com/mayermakes

facebook.com/mayermakes

twitter.com/mayermakes

instagram.com/mayermakes