Skip navigation
Adam Soileau

The Eyes Have it

Posted by Adam Soileau Oct 17, 2019
  This project took me a few weeks to complete mostly because of the minor learning curve for the IR transmitter and receiver on an Arduino. I used three IR sensors to track where a object was and then turned the two micro servos (with eyes attached) in that direction. I need to add that in the video, I accidentally referred to the batteries as lithium-Ion batteries when really they were lithium-polymer batteries.   I completed this using:   Arduino MKR ZERO Arduino MKR ZERO ...
Concept: I want to make a Halloween batman dog costume that has a flapping cape. I am going to use a continuous micro servo to pull the cape up and down, and use an accelerator to detect whether or not the dog is standing up or laying down, so that when the dog is standing up, the cape will flap, but when the dog is turned to the side, the cape will not move. I also plan on adding RGB LEDS around the batman symbol. I the costume to look like the cape is flapping in the wind when the dog is runni ...
Concept: I want to make a Halloween batman dog costume that has a flapping cape. I am going to use a continuous micro servo to pull the cape up and down, and use an accelerator to detect whether or not the dog is standing up or laying down, so that when the dog is standing up, the cape will flap, but when the dog is turned to the side, the cape will not move. I also plan on adding RGB LEDS around the batman symbol. I the costume to look like the cape is flapping in the wind when the dog is runn ...