• Intrinsic Safety - Battery Powered Electronic Design

    This discussion is mainly about equipment operating in hazardous locations. Basically, a shout out to engineers that are/were involved in similar projects. The standrad is known as ATEX (EU), Hazloc (NA).   Va...
    Profile Photo
    created by waleedelmughrabi
  • Which versions of raspberry pi are CE compliant ? Where do I find the CE Declaration of Conformity on this site ?

    Which versions of raspberry pi are CE compliant ? Where do I find the CE Declaration of Conformity on this site ?
    Profile Photo
    last modified by Elec_Engineer9999
  • 13465 Heatshrink :- Pro Power

    On part https://uk.farnell.com/pro-power/13645/heat-shrink-2-4mm-black-5m/dp/1008441?st=13645   What is the manufacturer and UL file number? If multiple suppliers can I have all.   Thank you Daniel
    Profile Photo
    created by rappinglove
  • DC analysis of a wideband amplifier

    Please help to do DC analysis and find the Q point parameters.
    Profile Photo
    last modified by sharuka
  • Functional Safety and ISO 26262 standard

    E/E systems in safety-critical markets (such as automotive, industrial, and medical) are becoming more complex as new designs are demanding an increase in the amount of advanced security and safety features, like fail...
    Profile Photo
    created by yoSoyTono
  • AD698 heating issue

    Hello,      I am using AD698 for my project. In that project, I am using micro-epsilon full bridge LVDT with excitation frequency of 5KHz and the effective voltage as 2.52V, I am using the same ci...
    Profile Photo
    last modified by ash09
  • Build a HDMI port switcher IR remote control

    Hello,   Recently i bought a 3-way HDMI switcher from ebay with a IR remote control but soon after the remote died. I am no electronics guy but, i was able to  check that IR LED was good as I de-soldered th...
    Profile Photo
    created by hiteshthappa
  • Power Circuit needed

    Dear All, I am looking to connect my adsl modem(12 V, 1A) directly to 12V ,30 A battery. Kindly suggest me a simple and the best method to control the large current flowing from the battery to avoid my modem power ci...
    Profile Photo
    last modified by inception007
  • PC0802LRS-AWA-B-Q (Order Code: 1671494 )

    Hello,   I am currently using this LCD display and I would like to know if this product is UL ?   Or EN 60950-1 ?   Only electrical data are given in the pdf file. No information about the CE confor...
    Profile Photo
    created by dli
  • control I/O pins of my PC USB

    hi i want to know how can i send some signal like  100101 or similar through my USB data ports to a output device.Like i want to use my pc to control some thing trough USB and seance USB do not have many io pins ...
    Profile Photo
    last modified by tanvir10
  • TRIM register in MC9s08mp16

    How to use the TRIM Register in this controller.? What is the use of TRIM Reg.?
    Profile Photo
    last modified by karuna1992
  • NEED A GUIDANCE IN SOME SENSORS.

    I need a sensor that can detect the motion from a long distance  I am using HCSR04 which has a range hardly to 7cm but need a range of 10-20 meters. If any one has any Idea which sensor to use then please let me ...
    Profile Photo
    last modified by prince587
  • Scuba diving regulatory requirements

    What regulatory process or certifications must an electronic scuba diving apparatus undergo? 
    Profile Photo
    last modified by pettitda
  • Need some book lists

    hello my name is tanvir i am studing in diploma in electronics in MITB Bangladesh.can any one help me in giving some list of books where i can find the topics about motherboard chip sets and south bridge and north bri...
    Profile Photo
    last modified by tanvir10
  • Are all ROHS and REACH type legislations consistent?

    Hello All, I am trying to understand the impact of such legislations on product configurations. I want to inquire if all of legislations pertaining to ROHS and REACH are consistent in terms of range of products they ...
    Profile Photo
    last modified by shumailmazahir
  • Certificate requirements for electronics startup or hobbyist

    Recently I have designed one of my idea into working product. I wanted to learn from expert how do small company or startup or hobbyist like me decides about regulation? Can you give an example of certification req...
    Profile Photo
    last modified by pathik
  • Unable to Flash BeagleBone Black (Rev C)

    I have Beaglebone Blck (Rev c) and I have flash BBB with the latest debian Image from BeagleBoard.org - latest-images    Under This link I have downloaded Image from below link Debian (BeagleBone Black - ...
    Profile Photo
    created by sachindawane
  • i wanna a magnetron that works on the way like a radar magnetron .i want to descover its waves in 5 kms distance

    i wanna a magnetron that works on the way like a radar magnetron .i want to descover its waves in 5 kms distance.may be guaid me that which frequnce can i use that can be detect on sensores 5kms and wich sensores cou...
    Profile Photo
    last modified by alikabir
  • Are you an EDE based near Cambridge, UK? Apply within…

    Do you work in the electronics engineering industry? Are you involved in ensuring your new products satisfy their legislative obligations? Do the terms Low Voltage Directive, Restriction of Hazardous Substances, Was...
    Profile Photo
    created by sleader
  • How can I get a 10 to 12 volt capacity battery with two input and output

    Dear Everyone in this community   Is it possible that a rechargeable battery may be it's more than one but two input and output port in that battery required. Elaborate: A battery with input port which take and...
    Profile Photo
    last modified by ronykhan