Skip navigation
Electronics Yorkshire is set to exhibit at Blundell’s Technology Week and miniexhibition between October 12 and 14 at the companies recently expanded showroom in Coventry.   Electronics Yorkshire will explain how companies can make use of the unique resources of test, analysis and repair equipment available in their Leeds centre, as well as the depth of training courses it can offer companies from all over the UK.   Electronics Yorkshire is the only IPC centre in the UK authori ...
Figures published by the Environment Agency show that the proportion of waste batteries collected for recycling in the UK rose from 9.15% in the first quarter of 2010 to 16.15% in the subsequent quarter.   The UK is therefore on track to achieve its first interim target to collect 10% of waste portable batteries for this year as the collection rate for the first half of the year was over 12%.   However, this remains work in progress as the first legally binding target set by the Euro ...
According to the ENDS Report the number of registrations under the EU’s REACH regime grew slightly during June and July but will have to increase ten-fold in the next few months to get anywhere near the totals expected by 30 November.   The European Chemicals Agency (ECHA) currently expects 25,000 to 75,000 registration dossiers to be submitted by this first deadline for existing, or phase-in, substances.   At the moment, 30% of dossiers submitted fail ECHA’s first &ldquo ...