• Altium Circuit Studio Development???

    My license for Circuit Studio has just come up for renewal, and after just double checking there has been next to no activity in the development world around Circuit Studio - is it worth renewing the license or is thi...
    Profile Photo
    last modified by engineereddownunder
  • How to make a component keepout that allows tracks?

    Hi, I'm using CS 1.5.2. I'm designing a PCB for a housing that has support pillars placed all over the PCB and need to be sure I don't place components in these areas. Tracks are OK. If I put the contact areas onto...
    Profile Photo
    last modified by bigbaldjohn
  • Can' t select PCB Part with cursor?

    I lost the ability to select a part with the mouse on a PCB.  I can't grab and move a part.  I can "box a part with the cursor", but can't select it  So I do see lines drawn around the part.. I think m...
    Profile Photo
    last modified by potterdog
  • Schematics are missing in 1.5.2 version

    Hi   I am using Circuit Studio 1.5.2 version.   During power outages, some schematics are missing or details are not displayed even though the project is compiled, saved.       Some compon...
    Profile Photo
    last modified by shastri
  • Polygon Pour on a power layer.

    I have four layer board and on the power layer, I want to create an area for +3V3 and +5V   But I cannot select the Power layer?   I must have done something wrong.   BUT it not allowing me to sele...
    Profile Photo
    last modified by lainscough_dfc
  • Design Rule Verification

    Hello. I make multilayer PCB with blind and buried vias. I have a problem with rule verification. The rules was made for each layers separately . That way is convenient for my design. for example 0.1mm: There...
    Profile Photo
    last modified by dmitriy2020
  • Multi part select not working to place a multiple componets.

    How do you select multiple components in shematic and place them on the PCB board. Cross probe does not do that for some reason, It alway brings me back to the schematic. When I select the PCB tab only one is highli...
    Profile Photo
    last modified by lainscough_dfc
  • Big cross on through hole

    Hello, I created 4-layer PCB and connect GND/VCC through hole to the internal plane layers. And I selected Direct Connect for Connect Style. What is this big green/blue cross on via? When I saw 3D view, electrical...
    Profile Photo
    last modified by tyro01
  • Is there an easier way to add a 3D rendering to a component rather than have to recreate the component in a library?

    I have been trying to add a 3D step file to an already existing part. From digging through all the help files and videos it appears this can only be done when creating a new part. Is there another way that I'm missing?
    Profile Photo
    last modified by sshaferdlm
  • How do you in PCB type in a part and place it

    How do you in PCB type in a part nmae (C2) and place it. There semms to be not find dialog or short cut.   This must be possible? It so simple
    Profile Photo
    last modified by lainscough_dfc
  • Wishlist for CS?

    In the hopes that CS continues to be maintained can we put together a wishlist for the developers?   For me I'd like to see:   Support for rooms.  It's great having hierarchial schematics but without ...
    Profile Photo
    last modified by motium
  • Step export produces empty file

    Hello,   I've finished a PCB and I'm generating the outputs.   Every component has its 3D model and the 3D view on Circuitstudio look great.   However, I'm not able to export the model as step to be ...
    Profile Photo
    last modified by csuser
  • Net labels not snapping to or joining electrical objects

    Normally, when you move a net label such that it's bottom left corner is touching an electrical object (i.e. a wire or the tip of a pin), an electrical connection is automatically made between the net label and the pi...
    Profile Photo
    last modified by jaza_tom
  • Supplier extensions

    Having trouble downloading the supplier extensions. From the My Acount->Extensions and Updates->Installed_Configure Platorm page. I select DigiKey or Mouser, and then apply. Circuit Studio reboots, and I get an...
    Profile Photo
    last modified by poobah
  • Getting a Refund?

    I bought a license for the tool last December to work on a client's assignment but this tool is full of bugs and I spend more time restarting the program after it crashes than doing useful work. It used to work after...
    Profile Photo
    last modified by alberto2033
  • Circuit Studio 1.5.2 Altium Part Provider will not load on installation or upgrade

    The Supplier Links have been broken in Circuit Studio.   When upgrading I got errors, so I did a complete uninstall and reinstall of Circuit Studio 1.5.2 (Build 30). The suggested supplier link mechanism is Alt...
    Profile Photo
    last modified by jwisepa
  • Issue starting new trial

    Hello!   I just downloaded CircuitStudio and was attempting to start a trial.  On the main page when I launch the application, it asks for my name/email/etc for the trial.  When I enter it and submit t...
    Profile Photo
    last modified by jvdt
  • Edit Board Shape

    I have a completed board and I noticed that when I view Board Information it says one of the sides is off by just a tiny bit. So, I went to click Edit Board Shape thinking I could click on the lines and have it snap i...
    Profile Photo
    last modified by Squintz
  • How do you hide 3D Models?

    I'm running DRC checks and some of the errors fall under 3D Parts. I know I can see the errors in 2D but I would also like to see them in 3D because sometimes they jump out at me more than in the 2D view. So, how can ...
    Profile Photo
    last modified by Squintz
  • How do I control polygon pour priority

    I'm pretty sure that I read there is not a dialog box to control the priorities and it doesn't appear that clicking send to back or bring to front has any real affect. So, what does control the priority?   I hav...
    Profile Photo
    last modified by Squintz