Skip navigation

HARTING

8 Posts authored by: martinbatin
Check out our step by step video guide to assembling a Han Modular connector!   Step 1:     Step 2:     Step 3:     Step 4:     Click here to browse our range ...
  At HARTING, our slogan ‘Pushing Performance’ challenges us to drive advancements across a range of industries. The Han® connector was first developed in the 1950’s and since then, the range has expanded and advanced, an ethos of continuous innovation that provides customers with simple yet reliable solutions.   The newest addition to the Han® portfolio is the Han® F+B, a range of connectors which have been specially designed for the requirements of ...
HARTING has over 70 years’ experience of producing robust industrial connectors. From the very beginning, the focus was always on developing a product which would be easy to handle, durable and adaptable for a range of uses. Another important consideration was an ethos of continuous innovation, which gives users reliable solutions even as markets and industries evolve.   In the case of the Han® 1A (Left), HARTING has recognised and responded to the demand for smaller interface ...
Christmas 4.0 - Episode 2 Click here for PushPull ...
Christmas 4.0 - Episode 1 Click here for ix Industrial® ...
Industry 4.0 is a hot topic, so it’s time to look at how we can integrate Industry 4.0 technologies across machinery, shop floor, and building management systems. To do so involves ensuring equipment is able to work with enhanced communication – including the three lifelines of industry – power, signal and data.   Multi-way communication of ‘big data’ is created by connecting devices so they are able to interact with each other. The modular industrial computin ...
Click here for a quick overview of the ix Industrial®   Ethernet is the undisputed dominant communication standard and as we increasingly rely on staying connected wherever we are, it is permeating ever more areas of our lives. As the demand for smaller, compact electronic and industrial devices grows, so connecting interfaces such as system cables must follow suit. However, whilst these components are reducing in size, they are simultaneously becoming more powerful to meet the demand ...
A secure fit with just one clickThere are many factors to consider when it comes to choosing a suitable connector for panels or control cabinets. Robustness, reliability and adaptability are all high on the list, but as businesses embrace more flexible production processes, simple handling and ease of use are becoming increasingly important. Control cabinets often contain a myriad of switches and connections, so the ability to quickly and efficiently disconnect and reconnect the industrial lifel ...