Skip navigation

HARTING

3 Posts authored by: penelope.stanton
In this blog I will briefly cover the standards that are pertinent to RFID transponders, and in particular those applicable to the memory bank of the transponder.   The most common applicable standards are EPC Class 1 Gen 2 and ISO 18000-6C.  The EPC standard is not exclusive to RFID transponders, but is also used extensively in barcode applications.     Read on to discover why standards affect transponder memory make-up, and what this means for applications by clicking this ...

Simplify RFID

Posted by penelope.stanton Jan 22, 2014
  This new blog series has the aim of informing, advising and giving best practice when implementing an RFID System. As with the adoption of any new technology, key concerns amongst new adopters include cost, lack of understanding of the benefits and pitfalls, and stories of failed applications and procedures.  E.g. What happens if I chose the wrong product to suit my application?   Over the coming months I will look to answer some of the questions with the aim to take the mystiq ...
The unique nature of the maritime environment takes a particularly heavy toll on the electrical components at work in offshore wind farms. The HARTING Technology Group has added the Han-Eco® series to its product range, creating another solution for this special application area.         The output from wind farms has risen steadily over recent years. Current plans envisage wind farms providing output up to 15 MW. If these facilities are to be utilized to the fullest ...