Skip navigation

Members

11 Posts authored by: Drew Fustini
Howdy,   Pumping Station: One member Steve Finkleman recently gave a lightning talk on how he is using the laser cutter at the space in his method to quickly fabricate circuit boards:     If you have any followup questions, then you can find him on Twitter at: http://twitter.com/IdeaPDish     Cheers, Drew ...
Howdy,   I cracked open the lastest issue of Make magazine this morning and was pleased to see Pumping Station: One featured!   The article can viewed in the digital edition of Make:   http://www.make-digital.com/make/vol29?pg=86#pg86     Cheers, Drew ...
Howdy,   Joe Born is a Pumping Station: One member and his company has just released a universal Android dock: "The dock charges via USB and gets sound from the headphone jack. Licensing beta technology from Sonr it also uses the headphone jack for data, allowing the remote control (and dock buttons) to control all your music apps (Pandora, Google Music, Amazon Cloud, etc). No app necessary if you’re content charging and controlling the device from the touch screen. Compatible with v ...
Drew Fustini

Biosensor Q & A

Posted by Drew Fustini May 19, 2011
Howdy,   Our biosensor array team was recently featured on the Make blog:   http://blog.makezine.com/archive/2011/05/gghc-semifinalist-profile-pumping-station-one.html   I really liked the answers that team member Shawn Blaszak wrote up but unfortunately they didn't make it into the Make post, so I figured I would post them here.   1. What was it like working on the GGHC challenge?   ANSWER:  Working on the challenge has been a lot of fun for me.  My mo ...
Howdy,   Our biosensor team is honored to be selected a finalist and humbled to be in the company of fellow finalists, Hackerspace Charlotte's Feltronics & BuildBrighton's Phonicubes.             I had a total "WOW!" moment when I realized, while watching the Feltronics video, that the circuit on the white board was a radio transmitter!  I think Feltronics will be a big help to electronics instruction everywhere including at hackerspaces.  And ...
Howdy,   The primary sensor I've been prototyping for the Pumping Station: One Biosensor Array is the galvanic skin response, or GSR, sensor.  GSR is a measurement of the electrical conductance of the skin.  Sweating causes changes in the conductance, which offers an indication of emotional excitement, because the sweat glands are controlled by the sympathetic nervous system.  GSR does not offer a fine grained indication of emotion, since it does not distinguish between the ...
Working feverishly down to the wire, we posted our final project status over on our own hackerspace blog and emailed our final documentation to the organizers in the nick of time.   Thanks so much to Mitch Altman, Mark and the rest of the Silverfox crew, and element14 for this wonderful opportunity!   Jordan Bunker, PS:One founding member & ReMade producer, was most excellent to stay up late with our biosensor team and took some great photos during our final integration demo (he ...
Our biosensor array team worked late into the night on Saturday at Pumping Station: One.  With the hackerspace challenge build deadline on Tuesday night, it's definately crunch time!   Thankfully we've got a nice array of working sensors (in the order of signal speed):   EKG Pulse oximeter GSR (Galvanic Skin Response) CO2 Temperature   Dan yet again played the role of test subject:   The QRD1114 sensor from SparkFun contains an IR LED and a compatible p ...
Howdy -   For the Great Global Hackerspace Challenge, our Pumping Station: One team is building a biosensor array. The array consists of sensors placed around one's body connected to an Arduino also attached to the body.  Software running on a computing device like a laptop or smartphone will visualize and log the biosignal data.  We decided the best way to connect the on-body Arduino to the computing device is via Bluetooth.   I'd like to give a brief overview of interf ...
Howdy -   Meet the Pumping Station: One team for the Great Global Hackerspace Challenge:     We're building a biosensor array!  Our team is using our hackerspace's wiki as the primary source for ongoing, day-to-day documentation:   http://wiki.pumpingstationone.org/index.php/Biosensor_Array   And we'll also be making regular posts to this blog to update on our progress and share the DIY techniques we are developing.     Cheers, Drew http://twitte ...
Howdy -   At Pumping Station: One, we're luckly to have several talented photograghers as members.  Here's a flickr photo sets featuring our hackerspace:   Anne Petersen (current President of PS:One) http://www.flickr.com/photos/opacity/sets/72157624089489776/     Kamil Krawczyk http://www.flickr.com/photos/kamil/collections/72157623324601656/     Photo by Anne Petersen     Photo by Kamil Krawczyk   Photo by Anne Petersen   Photo by An ...

Filter Blog

By date: By tag: