I finally received the 18650 batteries and charger that I ordered a while ago, so I can start building my AlphaBot https://www.element14.com/community/events/5782/l/arduino-day-workshop-nanodrone-ii-ai-and-computer-vision-with-lora-win…
I've got a lot going on in the next two months, so I probably won't get finished with this project for the contest - but I thought it would be fun to participate and start building this robot.
I am going to take the standard AlphaBot chassis and try to add some customization that I'll figure out on the fly
. The AlphaBot is an older (2017) Waveshare product that seems like an ideal platform for customization. It is configured to use an Arduino Uno Plus and a Raspberry Pi 3B, but it should be easily adapted to use other processors. The kit included an Uno Plus with a BlueTooth shield, so I'll get it running with that. Then I'll decide what modifications I want to make.
The AlphaBot is pretty simple. Two drive wheels with motors and a pivot roller. The drive axles are fitted with slotted disks, so that speed can be determined using a photo detector. I was initially surprised that there was so much mounting hardware (screws, nuts, standoffs, etc), but I soon realized that they had included two sets with the kit. Assembly was pretty easy with a little filing and lead trimming...
![]()
The top of the main PCB has two forward facing IR obstruction detectors (on the left) and just behind them are the two photo detector assemblies for the wheel disks.
![]()
The bottom of the main PCB holds the two motor assemblies and a line tracking sensor assembly at the rear.
![]()
The assembled unit with the wheels attached.
![]()
Next step is to program the Uno Plus and verify basic functionality.
Comments