Skip navigation
A tiny DC to DC buck converter board is useful for many applications, especially if it could deliver currents up to 3A (2A continuously without heatsink). In this article, we will learn to build a small, efficient, and cheap buck converter circuit.     References Full Article: https://www.pcbway.com/blog/technology/DC_to_DC_Buck_Converter_Adjustable__97__Efficient__3A.html MP2315 Library: https://componentsearchengine.com/part.php?partID=930350 Altium Plugin: https://www ...
Electronics & Design Projects Enter Your Electronics & Design Project for a Chance to Win Up to a $200 Shopping Cart of Product! About Project14 Project14 Home Monthly Themes Monthly Theme Poll     This is the first list in a five part series where we list the Greatest Hits of the Project14 as part of the first Makevember celebration on the element14 community in honor of the third Makevember event.  Makevember is an event that encourages everyone to spend 5 minutes a ...
Electronics & Design Projects Enter Your Electronics & Design Project for a Chance to Win Up to a $200 Shopping Cart of Product! About Project14 Project14 Home Monthly Themes Monthly Theme Poll   Beginning the last week of October, and throughout the month of November we will be celebrating the 3rd annual Makevember with the first ever Makevember on Project14.  You can read about Makevember 2019 in the following post: https://www.bricolage.run/blog/blog   Here is ...
Introduction: Components: Hardware: Software: Circuit Diagram: ARM MDK Code: Labview VI: Front Panel: Block Diagram: GUI v1.0: Demo: Images: Introduction: Solar power is the key source of green emission free energy. Every day, the sun gives us free of cost energy which is far more than we need to power everything on our earth. Solar power is widely used as a sole power source in off grid data gathering equipment or remote network nodes. So before a ...
      Features: Identify a fake Lithium-Ion/Lithium-Polymer/NiCd/NiMH battery Adjustable constant current load (can also be modified by the user) Capable of measuring the capacity of almost any kind of battery (below 5V) Easy to solder, build, and use, even for beginners (all components are Dip) An LCD user interface   Specifications: Board Supply: 7V to 9V(Max) Battery Input: 0-5V(max) – no reverse polarity Constant Current Load: 37mA to 540mA(max) – 16 Ste ...