Electronics & Design Projects

Enter Your Electronics & Design Project for a Chance to Win Up to a $200 Shopping Cart of Product!

About Project14

Project14 Home
Monthly Themes
Monthly Theme Poll

 

 

This is the first list in a five part series where we list the Greatest Hits of the Project14 as part of the first Makevember celebration on the element14 community in honor of the third Makevember event.  Makevember is an event that encourages everyone to spend 5 minutes a day working on projects to make things for the fun of it. The idea of a Greatest Hits compilation is borrowed from music.   On a Greatest Hits compilation you'll see 20-25 songs in no particular order and you'll notice a lot of gems missing if you're at all familiar with the artist's work. In the spirit of Makevember its not about whose project is "best", won prizes, and it is not a ranked or ordered list.   It's a celebration of the effort, the learning, the fun, the creativity, the skill, and the entertainment that you have provided to make this program possible.

 

We'll be releasing parts of the 25 54 greatest Hits of Project14 throughout Makevember and by the time we have finished this list, you'll have a representative sample of all the great work that's been done by the community members in support of this program.  The purpose is not to exclude but to celebrate, and the hope is that the 25 53 projects selected are representative of everything that's been going on around here since things got started.

 

Here is the first batch (Projects 25-20) of the 25 54 Greatest Hits on Project14:

 

The following Greatest Hits have been added to the list:

 

Check out more Greatest Hits from the element14 Community:

 

 

{tabbedtable} Tab LabelTab Content
Project 27: The Microbit Quartet

Project 027: The micro:bit Quartet  by jc2048

Clustered MCUs

This is a worthy entry that was entered after judging took place but was well worth the wait because it's awesome and it has to do with music. Using three yellow micro:bits, by kind permission of the Colchester Public Library, along a fourth micro:bit to create The micro:bit Quartet : four micro:bits playing music in unison!  Keeping things simple, he took advantage of the existing sound capability of the micro:bit but added an additional amplifier to drive miniature 8 ohm loudspeakers at a reasonable volume. Each micro:bit is monophonic and plays a single note at a time. Synchronisation between the microbits keeps them in time with one micro:bit acting as the conductor!

 

The micro:bit Quartet

 

 

 

 

Also on Project14 by jc2048:

Project 26: The Trickle Charger

Project 026: The Trickle Charger  by 14rhb

Energy Harvesting

 

In reality there are much better sources of wasted energy to get tapped into rather than the infrequent rainwater flow in a downpipe - light wind/breezes and solar will likely generate more energy over a longer period.

 

But for extra fun....then 14rhb  hopes you enjoy reading about the Trickle Charger. Such a turbine could be used where there is a fall in height of a stream but much simpler mechanisms like a water wheel would likely be a better choice...

 

The Trickle Charger

"This was a novel and interesting approach to energy harvesting.  Plenty of good examples of math, mechanics  and engineering were demonstrated throughout this project." - Community Member Judge

"14rhb  was the only one who attempted to harvest mechanical energy.  It was not an easy task, but he overcame most of the difficulties. Big points for the clever name, Trickle Charger.  He hand built a diode voltage multiplier, used a supercapacitor.  Most of all his background explanation was very informative, I liked that he quantified how much energy it takes for a "cuppa" tea.  We're used to milliamps and microamps for modern electronics on element14, you can't boil water with that." - Community Member Judge

"A 3D printed turbine! This is a super cool DIY project." - Community Member Judge

Recommended Product:

 

Product NameManufacturerQuantity
1.5F, 5.5v SupercapacitorKEMET Electronics 1Buy NowBuy Now

 

Product Name
3V DC Motor
1.5-4.5v DC Motor
Tektronix DMM TX3 Handheld Multimeter

 

Also on Project14 by 14rhb:

Project 25: Mini Gameboy Home Console

Project 25:  Mini Gameboy Home Console: The Gamebox DMG Consolizer  by nobble

A Question of Scale

 

 

This project came from the A Question of Scale competition.  The theme was to shrink or grow a project. Most people know Nobble from his custom handheld’s and unique video game mods, a few may remember him from his Hack Like Heck project. A fan since he was a kid, Ben Heck was the main source of inspiration for his projects and ideas for custom builds. The idea of portablizing a video game console or making a giant handheld device seemed too cliché so he decided to turn a small handheld into an even smaller home console.  He morphs Gameboy DGM-01 into a full-fledged Big Screen device thus playing off of both the "Shrink" AND "Grow" theme.

 

Mini Gameboy Home Console: The Gamebox DMG Consolizer from A Question of Scale

 

"This was a great project with an interesting, detailed blog and video giving a clear view of the design and build process. The end result was a very neat design that definitely rescaled the original." - Community Member Judge

 

 

"Mini Game Boy, great writeup, good walk through of design, and a solid build" - Community Member Judge

 

Recommended Products:

 

Product NameQuantity
Arduino Micro1Buy NowBuy Now

 

Product Name
Easy VGA
Gameboy DGM-01
Project 24: Arduino Powered MSE-6 (Mouse Droid)

Project 24:  Arduino Powered MSE-6 (Mouse Droid) by jomoenginer

Open Arduino

 

 

This project won the top prize in the Open Arduino competition so that right there tells you its not an ordered list.  Project14 chose to celebrate its birthday by celebrating Arduino Day with an Open Ended Arduino competition while also paying homage to the 25th anniversary of Star Wars: A New Hope.   If memory serves correct,  jomoenginer discovered he was the Grand Prize winner the same night he took his daughter to a Star Wars Movie.   The alignment of all these events was the Arduino Powered MSE-6 (a.k.a. Mouse Droid). For those of you who are not familiar, this is the little wheeled droid that Chewy roared at causing it to run off scared in A New Hope.  Apparently, there is a whole Mouse Droid Builders group and many examples of how to build this but most seem to be Radio Controlled.  His intent was to create a completely autonomous MSE-6 that can self navigate an area, as well as, go to a designated location. Based on Star Wars lore, these were maintenance droids used to perform minor repairs or as messenger bots which were voice activated to open and deliver a private message.  His version would include WiFi (and/or Bluetooth) where the Droid could be accessed remotely and given instructions for its next task.  To do this he set up a Mouse Droid webpage that was hosted on the Arduino Yun.  He was able to send a message to the Yun TFT screen, play the Mouse Droid sounds as well as control the droid by moving it Forward, Backward, Left, Right and Stop.   He added the ping sensor to the front but didn't use the sweep servo due to space. To create the body of the Mouse droid he used black foam board.  This was cheap and easy to work with, although he did some work to get the shape he was looking for. He took a few sheets and cut the individual pieces he needed. After hot cluing the pieces together, the Mouse Droid shape started to take form. With the chassis and the body together, it was time to put the guts (electronics) in the Droid. This included the Arduino Yun, Ardiuno UNO, Seeed TFT Screen, Speaker, 7.2 to 5 volt regulator, Steering servo, Photon Speed 2 Motor, and ESC.

 

 

Arduino Powered MSE-6 (Mouse Droid)

 

Recommended Products:

 

Product NameQuantity
Arduino Yun1Buy NowBuy Now
Arduino Uno1Buy NowBuy Now

2.8' TFT Touch Shield

1Buy NowBuy Now

7.2 to 5 Volt Regulator

1Buy NowBuy Now

Parallax Ping Sensor Board

1Buy NowBuy Now
Robotics Chassis1Buy NowBuy Now

 

Product Name
DuraTrax Photon Speed 2
Horizon ESC 60A ESC (Electronic Speed Controller)
Black Foam Board
Pluggable USB Audio
Speaker

 

Also on Project14  from jomoenginer :

Project 23: (Semi)Automated Plant Irrigation System

 

Project 23:  (Semi)Automated Plant Irrigation System by urkraft

Mixing Electronics & Water

 

This is an automated system for watering urkraft 's olive tree.  The main components for this are a soil moisture sensor, a 10 gallon bucket of water with a water level sensor, an Adafruit Feather HUZZAH ESP8266 microcontroller, and a peristaltic water pump.

 

The two sensors are connected to inputs of the feather, and the water pump is controlled by an output signal from the feather. There are two built in LED’s on the feather:

  • Red: used to indicate that the soil is dry enough to warrant watering
  • Blue: Used to indicate that the bucket is empty (requires a refill of water)

There are three criteria which all have to be met in order to turn on the pump (and water the plant):

  1. There must be water in the bucket
  2. The lack of moisture in the soil must be greater than a specified threshold value
  3. A specified minimum amount of time must have elapsed since the pump was last turned off while watering.

Any one of the following criteria will cause the pump to be turned off:

  • No water left in the bucket
  • The moisture level of the soil is higher than a specified threshold value (this criteria also triggers starting of the timer which keeps track of the amount of time that has elapsed since the pump was turned off).

 

(Semi)Automated Plant Irrigation System

"Well documented, clearly explained and with a good video showing both the making-of and the real-world application (very nice I should say)." - Community Member Judge

"A well executed build that included great features" - Community Member Judge

"Interesting project designed to keep an Olive tree alive and happy." - Community Member Judge

Recommended Products:

 

Product NameQuantity
Arduino Uno1Buy NowBuy Now
Adafruit Feather HUZZAH ESP82661Buy NowBuy Now

 

Product Name
5v 2.1A DC power supply w/micro usb contact
12v 1A DC power supply
Power Jack for the 12V Power Supply
Soil Moisture Sensor
water level switch NC
22k ohm 1/8w resistor
10k 1/8w resistor (quantity 2)
33 ohm 1/4w resistor
1N4001 diodes (quantity 2)
Peristaltic Pump
Breadboard
VR05R241A single pole DIL relay
Assorted jumper wires

 

Also on Project14 by urkraft:

 

 

{tabbedtable} Tab LabelTab Content
Project 22: Simple Solar Bot

Project 22: Simple Solar Bot by snidhi

Solar Power Devices

 

 

Simple Solar Bot

 

Simple Power Bot was conceived as a simple solar powered robot capable of harnessing energy from solar panels. Part of this project involved learning more about how an Arduino handled power consumption and whether it could get the voltage and current that it needed from solar power boards. What's really impressive, is the fact that this was snidhi 's first attempt working with solar energy, an undertaking that she was very enthusiastic about.  If everything goes according to plan, the Simple Solar Bot would be able to self sustain its energy requirements and be smart enough to go into sleep mode to consume less energy when there was no activity.  Adjustments were necessary throughout the process to nail down the right motors to use for the mechanical design.  This project involves an Arduino NaNo

 

"This project should be first place. It followed the theme and was completed. Being the first solar project by snidhi made it even better. ...Very detailed steps on how this project was created. From schematics, video, images and text. It could be re-made by many with the information included. ...Many uploaded videos detailing the continued progress throughout the project. The final video submission proves that it works and has a lot of potential. ...The project was original and very well planned. ...This being S Nidhi's first time working with solar power made it more impressive. There were some issues that were overcome with a couple of changes. ...Feedback was positive and encouraging." - Community Member Feedback

"This was a great lesson in overcoming deficiencies in initial plans and persevering to complete your goals". - Community Member Judge

 

"There was plenty of detail to follow, nice videos and a great sense of motivation." - Community Member Judge

Product NameQuantity
Arduino Uno1Buy NowBuy Now
Arduino Nano1Buy NowBuy Now
Fluke 179 Handheld Multimeter1Buy NowBuy Now

 

Product Name
Solar Panels (quantity 2)
Breadboard
L298N Dual H-Bridge Motor Driver
Analog 2-axis Thumb Joystick + Breakout Board
10W 3.7V LiPo Lithium Battery Charger
3.7V Li-Ion Lithium Battery Charger Protection Board
3.7V 2000mAh battery lithium polymer LiPo rechargeable battery
DC-DC Step Up Power Module Booster Power Module 3V-5V
Robotics Chassis
5 V Geared Motors
Sensors

 

Also on Project14 by snidhi :

Project 21: The Dancing Birds

Project 21:  The Dancing Birds by balearicdynamics

Clustered MCUs

 

This project was experiment to demonstrate that birds do not always have to be angry!  As balearicdynamics sets out to prove, they can do something else! He hypothesizes that birds can dance and that it is in fact possible to set up some sort of a small ecosystem where they can dance comfortably.  This project was chosen as the craziest project to use two or more microcontrollers.  It uses 6 micro servos and an Arduino Mega 2560 to control the motion and sync the servos.  The Arduino Mega was chosen because it has many pins, good speed, and a reasonable amount of programming memory and RAM.  With the Arduino Mega in control of The Dancing Birds , who was going to control the Arduino Mega?  balearicdynamics 's solution was none other than a BBC micro:bit!

 

 

 

For the grand prize I think the Dancing Birds is my favourite, inventive, funny and detailed write up. - Community Member Judge

Watching the video made my day. This is the type of project that  would brighten your day. It would be easy enough to re-create with different  objects that are meaningful to the creator. - Community Member Judges

Wonderful project with lots of care in its presentation, and documentation with photos and video too. This is a very inspiring project and I learned a lot from it. This is the level of inspiring projects I would like to be able to create, and aim to present it like that too one day, so really for me it was my favourite. - Community Members Judge

 

 

This was another creative project, where whimsy was on fully display. Sort of like Art runs into Engineering. - Community Member Judge

Creative, suited to the season, and fun.  Loved it. - Community Member Judge

 

Product NameQuantity
Arduino Mega 25601Buy NowBuy Now
BBC micro: bit1Buy NowBuy Now
Kitronik Edge connector1Buy NowBuy Now

Bitscope

1Buy NowBuy Now

 

Product Name
Six Micro Servos

 

Also on Project14 from balearicdynamics :

Project 021: Solar Panel Monitoring Using Particle Photon

Project 021:  Solar Panel Monitoring Using Particle Photon by ruchir1674

Remote Monitoring & Control

 

The aim of the project was to improve the efficiency of solar panels. The project is designed to supervise solar photovoltaic power generation to enhance the performance, monitoring and maintenance of the solar plant. With advancement of technologies the cost of renewable energy equipment is going down globally encouraging large scale solar photovoltaic installations. This massive scale of solar photovoltaic deployment requires sophisticated systems for automation of the plant monitoring remotely using web based interfaces as majority of them are installed in inaccessible locations and therefore are easy to be monitored from a dedicated location. The project allows monitoring power output of a solar panel, incident light intensity and the operating temperature.   In this project, the particle photon is interfaced with the voltage output pin of the solar panel, LM-35 temperature sensor and LDR sensor to monitor the power output, temperature and the incident light intensity respectively. A character LCD is also interfaced to the particle photon for real time display of the measured parameters. The Photon not only displays the measured parameters on the LCD screen, but also sends the measured values to the cloud server. For viewing the real-time data and logs sent by the board, the user needs to log in to the registered account from the Particle's official website.

 

Solar Panel Monitoring Using Particle Photon

"Solar Panel Monitoring, Great project, well described." - Community Member Judge

"This is a great project on a subject that is likely to have an impact on the future of energy generation. The blog was well detailed with a guide to the design, build and implementation of the project." - Community Member Judge

 

"The Solar Panel was technically the most proficient in using resources and the results were good." - Community Member Judge

 

 

Product NameQuantity
Particle Photon 1Buy NowBuy Now

 

Product Name
16x2 LCD
Solar Plate
LM-35 temperature sensor
LDR
Breadboard
Jumper wires

 

Also on Project14 from ruchir1674:

Project 022: Lock NFC

Project 022:  LockNFC  by Fred27:

NFC/RFID

 

Fred27 wanted his NFC/keypad lock to have many uses.  The garage door was the easiest as all I needed to do was simulate a button press. A loftier goal was to make something that fitted my front door. His requirements were that it must look professional with no dangling wires or bits duct taped to the back of the door, it must be possible to still use the normal key to open the door, any electronic failure must mean the door can be operated normally, and as you may have guessed there was the WAF  (Wife Acceptance Factor).  For the PCB design he wanted an NFC reader that was tuned to his NFC implant and which also included a keypad for his (unmodified) kids to use.  After waiting for the PCB to arrive from Seed, it was time to populate it, run it through the toaster oven and see if there were any mistakes made. As usual, QFN soldering of the TRF7970A NFC transceiver was a struggle. The final result looks professional enough with the naked eye even if the process certainly wasn't. You can't really test the hardware without some firmware running on the microcontroller, so he quickly adapted my test code from the development board. It wasn't too long until he had the capacitive touch button code running and working. Then he got the NFC code reading an NFC tag. It's all very well deciding that the PCB itself will be the front panel for the lock, but it will still need an enclosure. He decided to tackle the simplest lock first - and that was his garage door. The reason for this is that all he has to do is simulate a button press, At worst a relay across the existing push-button would do. Of course, that still leaves the issue of how to mount it outside the garage. Once again, this is probably the simplest use case. He can go with a 3D printer box and route the cable straight through the single-skin brickwork of my garage. Being a coder at heart, his tool of choice for 3D modelling is OpenSCAD. It's very different from the more artistic modelling tools, but particularly suits a parametric design.  He has a "normal" UK lock or nightlatch on the front door. They work pretty well, but it’s a little trickier to attach a motor to what appears to be a more common lock in the US - the deadbolt.

 

LockNFC

"LockNFC was an innovative project that successfully overcame several engineering challenges. Fred27  gave clear step-by-step instructions in a well-written series of blogs, complete with photos and videos. I liked that the project objectives and design criteria were clearly set out at the beginning." - Community Member Judge

"I thought this was the most practical project, one that would be used all the time.  I also felt this had the most "finished" packaging (very nice PCB as the front panel).  And there were multiple functional variants based on the same basic hardware (good design reuse)." - Community Member Judge

"For a Project14 project I enjoyed watching this one come together the most was very cool" - Community Member Judge

 

 

"I know David has put a lot of effort into this over several years, sometimes I mark down if a project isn't created just for that month's Project14, and the same was true here. But all the other areas of David's project attracted so many other points in my marking he still managed a very good score ! The project is great as it contains a custom PCB, 3D printing of lock components (never seen that tried before) and I do believe he even has an RFID embedded in his hand !" - Community Member Judge

"Project executed very well both by design and architecture. An interesting approach to the problem the author has set all the components from mechanics hacks to case design and a good aesthetic. An advanced maker build." - Community Member Judge

"This was a great project with lots of technical details provided in multiple, well laid out blogs. The video showed a fully functioning project with a professional finish, it makes me wonder how long something it will be before something like this will commercially available." - Community Member Judge

 

Also on Project14 by Fred27:

 

 

{tabbedtable} Tab LabelTab Content
Project 023: Infinity  Living Christmas Wreath

Project 023: Infinity Living Christmas Wreath  by  dwinhold

The Holiday Special

 

The Infinity Living Christmas Wreath was done as a family project. Dale made this with his kids. They wanted to make something unique and what they came up with was awesome!

 

To create the wreath they used 144 RGB LED light string, an Arduino, a Raspberry Pi, Screen, speakers, 2 pieces of one way mirror and a 12 volt transformer.  The LED strip was placed between the one way mirrors. The Arduino is used to control the LED pattern and the transformer is used to power the LED's. Meanwhile, the Raspberry Pi and screen is used to display the burning log behind the mirror with speakers for fire crackling sound.

 

Infinity Living Christmas Wreath

"Unique idea for a Christmas artifact. ...the result is beautiful."

 

 

"If I win the grand prize I would keep the 3d printer and use it to make small toys for kids to enjoy. The SAM's STEAM KIT will be given to my sons school for their computer science class. This is a way to help many students with a single (incredible) gift.

 

Whom ever wins this challenge, the donation of the gifts is truly the spirit of the holidays!!

 

Merry Christmas and/or Happy Holidays everyone!!"  - dwinhold

Project 024: BoneCommander - A Ruggedized BeagleBone Linux Computer

Project 024:  BoneCommander - A Ruggedized BeagleBone Linux Computer  by  ninjatrent

Portable Electronics Kit

The BoneCommander by ninjatrent  is a rugged and mobile BeagleBone Linux Computer powered by a BeagleBone Black Wireless SBC. An element14 BeagleBone 4.3" LCD Display Cape is the primary display interface for the BBB W.

 

There is a 4 port USB Hub connected to the USB Host on the BeagleBone and a Wireless USB Keyboard with touchpad connected to this USB Hub. Power is provided by an Adafruit PowerBoost 1000C 5V Lipo USB Boost Charger and a 3.7v 2500mAh Lithium Ion Polymer Battery. The PowerBoost 1000C utilizes the TPS61090 boost converter from TI.

 

 

BoneCommander - A Ruggedized BeagleBone Linux Computer

 

 

Product NameQuantity
BeagleBone Black Wireless1Buy NowBuy Now
BeagleBone 4.3 LCD Display1Buy NowBuy Now
Miniature Wireless USB Keyboard with Touchpad1Buy NowBuy Now

 

Product Name
Zero4U - 4 Port USB Hub for Raspberry Pi Zero v1.3
PowerBoost 1000 Charger - Rechargeable 5V Lipo USB Boost @ 1A - 1000C
Lithium Ion Polymer Battery - 3.7v 2500mAh
Debian 9.3 2018-01-28 4GB SD IoT

 

Also on Project14 from ninjatrent:

Project 025: My late (and incomplete) entry for the Portable Electronics Kit - The Pi-IDE (Pie-Eyed).

Project 025:  My late (and incomplete) entry for the Portable Electronics Kit - The Pi-IDE (Pie-Eyed).  by the-dubster

Portable Electronics Kit

 

After the-dubster  watched  Episode 231: Ben Heck’s Lunch Box Dev Kit Episode  he thought to himself  "I could do with one of those - but a bit different."

 

The Dev Kit was great for boards that had a video output, but it wasn’t so useful for an Arduino  -  the-dubster  needed something that he could use to program the Arduino as well as practice his Dev skills on . . . he needed a laptop type sort-of-device!

 

He presents his idea for a RPi 3 based Portable dev / electronics kit: The Pi-IDE.

My late (and incomplete) entry for the Portable Electronics Kit - The Pi-IDE (Pie-Eyed).

 

 

"I appreciate the effort of building a kit into a briefcase. This is a truly portable electronics kit " - Community Member Judge

 

Project 026: Fancy Eye

Project 026: Fancy Eye by armour999

Electronic Toys

 

Fancy Eye is a roving robot with the Maix Go Board for Machine Vision.  armour999  brushed off her Gertbot and attached it to a Raspberry Pi 3. Software can be uploaded to the Maix Go using Arduino !

 

Fancy Eye

 

 

Also on Project14 by armour999 :

Project 027:  Process Duration Timer

Project 027: Process Duration Timer  by jw0752

DIY Test Equipment

 

 

 

"A well defined project that met all the objectives. It used cheap and readily available parts which were repurposed to suit the project." - Anonymous Judge

 

"Timing events can be really important in a lab, and this project was unique in that it took a low-cost circuit (a clock) and transformed it into a timer in a very unique way. Then John extended it further by using an Arduino to control it based on voltage thresholds. It would be very useful for anyone wishing to characterise a battery or capacitor." - Anonymous Judge

 

"If I had to vote for just one, it would be the Process Duration Timer, because it is something I've always wanted to make for myself too, a timer for measuring things in the lab." - Anonymous Judge

 

This was a universal pick from all the community members that were asked to help pick a piece of DIY Test Equipment as you can see from the comments above. Its part of a 4-part blog series from jw0752 and it was a favorite of the judges because they could appreciate the importance of a timer for measuring things in the lab. The final entry is highlighted here but you can view the entire series on the  DIY Test Equipment page:

 

Also on Project14 by jw0752 :