Skip navigation
kk99

Infrared thermometer

Posted by kk99 Nov 15, 2017
I would like to show you a infrared thermometer with MLX90614 sensor, seven segment display HP QDSP-6040 and ATtiny2313 MCU. Sensor allow to measure temperature in following ranges: 1) -40 - 125 °C - in case of measurement of sensor temperature, 2) -70 - 380 °C - in case of measurement of object temperature. In project is implemented only measurement of object in Celsius degrees.   ATtiny2313 MCU communicates with sensor by SMBus. Measured value of temperature is shown on disp ...