Skip navigation
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   Although not directly related to fighting germs or Covid-19 this project is about enhancing well being. During the lockdown we were allowed one outside period of exercise each day. I decided that I would have mine early in the morning ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   My entry for fighting germs. A self cleaning, easy disinfect mask based around element 29, complete with some Bob Ross crafting. I attempt to airbrush metal powder in the video below and explain some of the more important reasons for w ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   1 Skip and Work with CubeMX 2 FreeRTOS and CMSIS_RTOS_2 3 The interface with GFX 4 The How to use this smart home hub, 4 Hardware control and demo 5 Further to Go 1 Skip and Work with CubeMX TouchGFX works f ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   This is a DIY timer that ensures you wash your hands for at least 20 seconds, which is proven to kill the coronavirus. Why make this timer instead of just singing "Happy Birthday" twice? Because it's fun to engineer your own custom solu ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   GUI--FightingGerms 1 Problem to solve 2 Component to be used 3 Program Flow 4 GUI with TouchGFX 5 Hardware Porting with CubeMX 6 Next Codes and Components of Fighting_germ_at_home 1 Problem to solve 1.1 Du ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   It’s during times like these that inspire innovation. Like the announcements below.   In that spirit, the "Fighting Germs” contest is here to not only reward that innovation ─ but also give to other charities for thos ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   The system is designed to detect unauthorized entry (face masks), that are essential to protect ourselves and to avoid spreading COVID-19.   Things used in this projectHardware Components NVIDIA Jetson Nano Developer Kit x 1 Ras ...
dennisy

Covid Floor Disinfector

Posted by dennisy Jun 1, 2020
Hi All, Here is my project; Autonomous floor disinfector in the house which can wake you up by ramming into your bedroom door. It's been a bit rough since the restrictions of UVC LED components has been enforced by most of the countries. So for the time being, I may end up using UVA or UVB LEDs, but hey, since they are swappable, I will just keep punching through. Below I shared a work in progress from my Kicad, I recently learned how to use it thanks to Shawn from Digikey for the lovely video t ...
Fighting Germs Enter Your Project for a Chance to Win a Thermal Imaging Camera, Germicidal UV Lamp, and a Shopping Cart with Matching Charity Donation! Submit an EntrySubmit an Entry  Back to homepage Project14 Home Monthly Themes Monthly Theme Poll   My project is EMDR tappers made with Arduino UNO. It falls under the category Build Projects to Help You (and others) Cope!    EMDR is used by psychotherapists in the office setting to reduce patients’ stress and an ...