Merry Boxes & LEDs

Enter Your Project for a chance to win a Maker Tool Kit, an Oscilloscope Grand Prize for the project that brings the Most Joy to the Heart, and Gift to Gives!

Back to The Project14 homepage

Project14 Home
Monthly Themes
Monthly Theme Poll

 

tree

I would like to present a small Christmas tree made from 15 WS2812B LEDs connected to attiny13 MCU. Tree is made from 5 stripes with 5, 4, 3, 2 and 1 LEDs. LEDs are driven from single pinout PB4 of Attiny13 MCU. Below is schematic:

schematic

MCU was put in cartridge from 35mm tape. As power supply I have used 5V from USB. Code is written in C with usage of light_ws2812 library. Below there is output from compilation:

build

There are five different effects for which we could modify brightness and delay. Below are few more photos:

tree2

tree3

tree4

tree5

Source code is available in attachment. Below there is short video presentation:

Second video recorded with different camera setting: